Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Programming Cost Optimized XC7Z020 via JTAG
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 335 subscribers
  • Views 369 views
  • Users 0 members are here
Related

Programming Cost Optimized XC7Z020 via JTAG

Former Member
Former Member over 10 years ago

Several months ago I purchased the cost optimized versions of the XC7Z020 boards. After realizing my mistake, I went through the BOM to get a list of the parts I needed to install to allow programming of the boards via JTAG. As far as I can tell all I need is:


D6  -  BAS21        Fast Switching Diode
J3  -  87832-1420   7x2 Shrouded Header
JT1, JT2, JT3 (set to JTAG mode)



I'll be powering the board through a breakout card so the installing the diodes pertaining to power are unnecessary.



I am trying to take a project that I have working on an XC7Z010 board and use it on the '20' board. After going into Vivado and changing the part number from '10' to '20', regenerating a bitstream, exporting that to SDK, and attempting to program the board I get a "Target List is Empty" Error. In the "Program FPGA" menu I can switch the 'Device' field from auto-detect to the XCZ7020 board, but I still get a 'Target List is Empty'.



Does anyone have any ideas? Have I installed the correct parts to program the cost-optimized boards via JTAG or have I missed something?


  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 10 years ago

    After a quick look at the schematic you seem to have added the required parts.

     

    You might try building a project for the MicroZed 7020 from the beginning to rule out an error made in modifying the project. Even a simple hello world or peripheral test application would work to test out your modified boards.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 10 years ago

    You could also try out the solution from the Zynq Tutorials posted. A solution for the MicroZed 7020 is provided.

    Bryan