I think this is a JTAG connection issue. When running the lab 2 portion of the Speedway Tutorial for the MicroZed board, I cannot get the board to be found to run the program.
This is Experiment 4, step 16 of the "Developing Zynq-7000 All Programmable SoC Hardware (Vivado 2015.2 and 2016.2)" [| Zedboard ]
The result is an Error Launching Program message:
I am running Vivaldo 2018.3 and Xilinx SDK 2018.3 on a Windows 10 PC. I am using the Digilent JTAG-HS3 Programming cable.
Also tried running the Hardware Manager under Vivado, and it claims "No hardware target is open." When I select "Open target" and select "Auto Connect" is shows localhost(0) with a status of Connected
Can anyone help me troubleshoot this problem?