Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design EMIO voltage level in zynq
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 336 subscribers
  • Views 1469 views
  • Users 0 members are here
Related

EMIO voltage level in zynq

sarankk
sarankk over 4 years ago

Is  it possible to configure EMIO pins of zynq 7000 to 1.8 volts?

  • Sign in to reply
  • Cancel
  • bhfletcher
    bhfletcher over 4 years ago

    There are no EMIO pins, per se. EMIO is the internal channel between the PS and PL, which may or may not be pinned out to a physical pin. If you are talking about an EMIO channel that is pinned out to a physical PL pin, then the voltage definition of that pin is governed by the type of PL pin that it is.

     

    On Zynq-7000, there are two types of PL I/Os -- HR and HP. You can see the voltage I/O characteristics in DS191. Both can support 1.8V.

    image

     

    Are you asking specifically about whether the Mini-ITX can set a PL Pin to 1.8V? Looks like Bank 35 is set to 1.8V. Banks 10, 11, 12, and 13 can be set to 1.8V if you short 3-5 on JP7.

     

    Bryan