Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Looking for defconfig for uboot and kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 355 subscribers
  • Views 1213 views
  • Users 0 members are here
Related

Looking for defconfig for uboot and kernel

e14 Contributor
e14 Contributor over 10 years ago

Hello,

Could someone please point me in the correct direction to find the u-boot defconfig and Linux defconfig files for the Mini-ITX XC7Z045 board?  It does not appear they are in the Linux mainline or in the Xilinx OSL mainline.

configs within u-boot-xlnx mainline @ master:

-rw-rw-r-- 1 tduffy tduffy  210 Apr 19 12:29 configs/zynq_afx_nand_defconfig
-rw-rw-r-- 1 tduffy tduffy  289 Apr 19 12:29 configs/zynq_afx_nand_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  179 Apr 19 12:29 configs/zynq_afx_nor_defconfig
-rw-rw-r-- 1 tduffy tduffy  258 Apr 19 12:29 configs/zynq_afx_nor_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  369 Apr 19 12:29 configs/zynq_afx_qspi_defconfig
-rw-rw-r-- 1 tduffy tduffy  448 Apr 19 12:29 configs/zynq_afx_qspi_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  399 Apr 19 12:29 configs/zynq_cc108_defconfig
-rw-rw-r-- 1 tduffy tduffy  268 Apr 19 12:29 configs/zynq_cse_nand_defconfig
-rw-rw-r-- 1 tduffy tduffy  266 Apr 19 12:29 configs/zynq_cse_nor_defconfig
-rw-rw-r-- 1 tduffy tduffy 1187 Apr 19 12:29 configs/zynq_cse_qspi_defconfig
-rw-rw-r-- 1 tduffy tduffy  544 Apr 19 12:29 configs/zynq_microzed_defconfig
-rw-rw-r-- 1 tduffy tduffy  342 Apr 19 12:29 configs/zynq_picozed_defconfig
-rw-rw-r-- 1 tduffy tduffy  675 Apr 19 12:29 configs/zynq_zc702_defconfig
-rw-rw-r-- 1 tduffy tduffy  697 Apr 19 12:29 configs/zynq_zc702_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  590 Apr 19 12:29 configs/zynq_zc706_defconfig
-rw-rw-r-- 1 tduffy tduffy  612 Apr 19 12:29 configs/zynq_zc706_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  676 Apr 19 12:29 configs/zynq_zc770_xm010_defconfig
-rw-rw-r-- 1 tduffy tduffy  608 Apr 19 12:29 configs/zynq_zc770_xm010_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  440 Apr 19 12:29 configs/zynq_zc770_xm011_defconfig
-rw-rw-r-- 1 tduffy tduffy  297 Apr 19 12:29 configs/zynq_zc770_xm011_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  410 Apr 19 12:29 configs/zynq_zc770_xm012_defconfig
-rw-rw-r-- 1 tduffy tduffy  342 Apr 19 12:29 configs/zynq_zc770_xm012_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  596 Apr 19 12:29 configs/zynq_zc770_xm013_defconfig
-rw-rw-r-- 1 tduffy tduffy  394 Apr 19 12:29 configs/zynq_zc770_xm013_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  534 Apr 19 12:29 configs/zynq_zed_defconfig
-rw-rw-r-- 1 tduffy tduffy  518 Apr 19 12:29 configs/zynq_zed_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  594 Apr 19 12:29 configs/zynq_zybo_defconfig

configs within linux-xlnx mainline @ master:

-rw-rw-r-- 1 tduffy tduffy 5721 Apr 19 12:31 arch/arm/configs/xilinx_zynq_defconfig

I suspect that using the xilinx_zynq_defconfig is fine for the time being as a base-line.  I don't think that is my issue.  I do, however, have a problem where I can not get u-boot to boot correctly.  I suspect this is due to not having the correct defconfig.

Any support is greatly appreciated.

Thanks,

-TD

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Tim,

      It is on our list to get these configurations added to mainline, but for the moment I have only a partial solution for you.  If you look under the Ubuntu reference design for the Zynq Mini-ITX, you will see a U-boot Update document.  That describes the procedure for how to create a defconfig file for Zynq, and includes the file for the Xilinx 2015.3 release.

    For the kernel defconfig, there is a chapter in the Ubuntu manual that describes how to create that from an existing defconfig.  But we don't have a finished solution for that one.

    So it will take a little work on your part, but most of what you need is already done.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Awesome!  Thanks Ron.  I'll dive in right now and report back my findings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    No such luck with the modifications :/ ...

    FSBL executes, and the PL is programmed, but then nothing is displayed on the UART.  I tested the SD Card with a BOOT.BIN with a HelloWorld application, so I'm fairly confident that isn't the issue.

    I suppose it could be an issue with the PL.  I'll continue investigating that.

    Any chance you have a known working u-boot 2015.3 binary laying around?

    Thanks,

    -TD

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi Tim,

    Are you testing HelloWorld on the same hardware platform and PS configuration as you are with U-Boot?  Is it possible that your hardware platform (ps7_init) is incorrectly configuring the UART?

    Take a look here:

    http://www.wiki.xilinx.com/Zynq+Releases

    I would think that the absence of a 2015.3 release is some sort of clue that there were problems (perhaps in U-Boot) around the time of the tools release.

    Are you able to try a more recent version of tools like 2015.4 instead?

    Regards,

    -Kevin