Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Looking for defconfig for uboot and kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 345 subscribers
  • Views 1029 views
  • Users 0 members are here
Related

Looking for defconfig for uboot and kernel

Former Member
Former Member over 9 years ago

Hello,

Could someone please point me in the correct direction to find the u-boot defconfig and Linux defconfig files for the Mini-ITX XC7Z045 board?  It does not appear they are in the Linux mainline or in the Xilinx OSL mainline.

configs within u-boot-xlnx mainline @ master:

-rw-rw-r-- 1 tduffy tduffy  210 Apr 19 12:29 configs/zynq_afx_nand_defconfig
-rw-rw-r-- 1 tduffy tduffy  289 Apr 19 12:29 configs/zynq_afx_nand_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  179 Apr 19 12:29 configs/zynq_afx_nor_defconfig
-rw-rw-r-- 1 tduffy tduffy  258 Apr 19 12:29 configs/zynq_afx_nor_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  369 Apr 19 12:29 configs/zynq_afx_qspi_defconfig
-rw-rw-r-- 1 tduffy tduffy  448 Apr 19 12:29 configs/zynq_afx_qspi_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  399 Apr 19 12:29 configs/zynq_cc108_defconfig
-rw-rw-r-- 1 tduffy tduffy  268 Apr 19 12:29 configs/zynq_cse_nand_defconfig
-rw-rw-r-- 1 tduffy tduffy  266 Apr 19 12:29 configs/zynq_cse_nor_defconfig
-rw-rw-r-- 1 tduffy tduffy 1187 Apr 19 12:29 configs/zynq_cse_qspi_defconfig
-rw-rw-r-- 1 tduffy tduffy  544 Apr 19 12:29 configs/zynq_microzed_defconfig
-rw-rw-r-- 1 tduffy tduffy  342 Apr 19 12:29 configs/zynq_picozed_defconfig
-rw-rw-r-- 1 tduffy tduffy  675 Apr 19 12:29 configs/zynq_zc702_defconfig
-rw-rw-r-- 1 tduffy tduffy  697 Apr 19 12:29 configs/zynq_zc702_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  590 Apr 19 12:29 configs/zynq_zc706_defconfig
-rw-rw-r-- 1 tduffy tduffy  612 Apr 19 12:29 configs/zynq_zc706_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  676 Apr 19 12:29 configs/zynq_zc770_xm010_defconfig
-rw-rw-r-- 1 tduffy tduffy  608 Apr 19 12:29 configs/zynq_zc770_xm010_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  440 Apr 19 12:29 configs/zynq_zc770_xm011_defconfig
-rw-rw-r-- 1 tduffy tduffy  297 Apr 19 12:29 configs/zynq_zc770_xm011_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  410 Apr 19 12:29 configs/zynq_zc770_xm012_defconfig
-rw-rw-r-- 1 tduffy tduffy  342 Apr 19 12:29 configs/zynq_zc770_xm012_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  596 Apr 19 12:29 configs/zynq_zc770_xm013_defconfig
-rw-rw-r-- 1 tduffy tduffy  394 Apr 19 12:29 configs/zynq_zc770_xm013_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  534 Apr 19 12:29 configs/zynq_zed_defconfig
-rw-rw-r-- 1 tduffy tduffy  518 Apr 19 12:29 configs/zynq_zed_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy  594 Apr 19 12:29 configs/zynq_zybo_defconfig

configs within linux-xlnx mainline @ master:

-rw-rw-r-- 1 tduffy tduffy 5721 Apr 19 12:31 arch/arm/configs/xilinx_zynq_defconfig

I suspect that using the xilinx_zynq_defconfig is fine for the time being as a base-line.  I don't think that is my issue.  I do, however, have a problem where I can not get u-boot to boot correctly.  I suspect this is due to not having the correct defconfig.

Any support is greatly appreciated.

Thanks,

-TD

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 9 years ago

    Hi Tim,

      It is on our list to get these configurations added to mainline, but for the moment I have only a partial solution for you.  If you look under the Ubuntu reference design for the Zynq Mini-ITX, you will see a U-boot Update document.  That describes the procedure for how to create a defconfig file for Zynq, and includes the file for the Xilinx 2015.3 release.

    For the kernel defconfig, there is a chapter in the Ubuntu manual that describes how to create that from an existing defconfig.  But we don't have a finished solution for that one.

    So it will take a little work on your part, but most of what you need is already done.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    Hi Tim,

      It is on our list to get these configurations added to mainline, but for the moment I have only a partial solution for you.  If you look under the Ubuntu reference design for the Zynq Mini-ITX, you will see a U-boot Update document.  That describes the procedure for how to create a defconfig file for Zynq, and includes the file for the Xilinx 2015.3 release.

    For the kernel defconfig, there is a chapter in the Ubuntu manual that describes how to create that from an existing defconfig.  But we don't have a finished solution for that one.

    So it will take a little work on your part, but most of what you need is already done.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Awesome!  Thanks Ron.  I'll dive in right now and report back my findings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    No such luck with the modifications :/ ...

    FSBL executes, and the PL is programmed, but then nothing is displayed on the UART.  I tested the SD Card with a BOOT.BIN with a HelloWorld application, so I'm fairly confident that isn't the issue.

    I suppose it could be an issue with the PL.  I'll continue investigating that.

    Any chance you have a known working u-boot 2015.3 binary laying around?

    Thanks,

    -TD