Hello,
Could someone please point me in the correct direction to find the u-boot defconfig and Linux defconfig files for the Mini-ITX XC7Z045 board? It does not appear they are in the Linux mainline or in the Xilinx OSL mainline.
configs within u-boot-xlnx mainline @ master:
-rw-rw-r-- 1 tduffy tduffy 210 Apr 19 12:29 configs/zynq_afx_nand_defconfig
-rw-rw-r-- 1 tduffy tduffy 289 Apr 19 12:29 configs/zynq_afx_nand_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 179 Apr 19 12:29 configs/zynq_afx_nor_defconfig
-rw-rw-r-- 1 tduffy tduffy 258 Apr 19 12:29 configs/zynq_afx_nor_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 369 Apr 19 12:29 configs/zynq_afx_qspi_defconfig
-rw-rw-r-- 1 tduffy tduffy 448 Apr 19 12:29 configs/zynq_afx_qspi_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 399 Apr 19 12:29 configs/zynq_cc108_defconfig
-rw-rw-r-- 1 tduffy tduffy 268 Apr 19 12:29 configs/zynq_cse_nand_defconfig
-rw-rw-r-- 1 tduffy tduffy 266 Apr 19 12:29 configs/zynq_cse_nor_defconfig
-rw-rw-r-- 1 tduffy tduffy 1187 Apr 19 12:29 configs/zynq_cse_qspi_defconfig
-rw-rw-r-- 1 tduffy tduffy 544 Apr 19 12:29 configs/zynq_microzed_defconfig
-rw-rw-r-- 1 tduffy tduffy 342 Apr 19 12:29 configs/zynq_picozed_defconfig
-rw-rw-r-- 1 tduffy tduffy 675 Apr 19 12:29 configs/zynq_zc702_defconfig
-rw-rw-r-- 1 tduffy tduffy 697 Apr 19 12:29 configs/zynq_zc702_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 590 Apr 19 12:29 configs/zynq_zc706_defconfig
-rw-rw-r-- 1 tduffy tduffy 612 Apr 19 12:29 configs/zynq_zc706_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 676 Apr 19 12:29 configs/zynq_zc770_xm010_defconfig
-rw-rw-r-- 1 tduffy tduffy 608 Apr 19 12:29 configs/zynq_zc770_xm010_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 440 Apr 19 12:29 configs/zynq_zc770_xm011_defconfig
-rw-rw-r-- 1 tduffy tduffy 297 Apr 19 12:29 configs/zynq_zc770_xm011_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 410 Apr 19 12:29 configs/zynq_zc770_xm012_defconfig
-rw-rw-r-- 1 tduffy tduffy 342 Apr 19 12:29 configs/zynq_zc770_xm012_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 596 Apr 19 12:29 configs/zynq_zc770_xm013_defconfig
-rw-rw-r-- 1 tduffy tduffy 394 Apr 19 12:29 configs/zynq_zc770_xm013_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 534 Apr 19 12:29 configs/zynq_zed_defconfig
-rw-rw-r-- 1 tduffy tduffy 518 Apr 19 12:29 configs/zynq_zed_RSA_defconfig
-rw-rw-r-- 1 tduffy tduffy 594 Apr 19 12:29 configs/zynq_zybo_defconfig
configs within linux-xlnx mainline @ master:
-rw-rw-r-- 1 tduffy tduffy 5721 Apr 19 12:31 arch/arm/configs/xilinx_zynq_defconfig
I suspect that using the xilinx_zynq_defconfig is fine for the time being as a base-line. I don't think that is my issue. I do, however, have a problem where I can not get u-boot to boot correctly. I suspect this is due to not having the correct defconfig.
Any support is greatly appreciated.
Thanks,
-TD