Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Ethernet only working in Gigabit mode (not 100Mbit/s)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 343 subscribers
  • Views 756 views
  • Users 0 members are here
Related

Ethernet only working in Gigabit mode (not 100Mbit/s)

Former Member
Former Member over 11 years ago

I have a Gigabit ethernet card in my primary development computer. When I connect the Mini-ITX Zynq board directly to that (with static IPs on both), it works fine (testing with "ping <address>". However, if it connects through a 10/100Mbit/s switch, it fails to work. Similarly, another development computer with only a 10/100Mbit/s ethernet card directly connected does not work. This makes me conclude that ethernet in anything less than 1Gbit/s mode on the Mini-ITX does not work. I am using the stock standard microSD to boot up. I have also built up my own Linux kernel and image, which also has exactly the same issue.

I also have a Zedboard. With the stock standard SD to boot up, this does work in 100Mbit/s mode through the switch, and with the 100Mbit/s ethernet card in the development computer.

Is this a limitation of the hardware, or is it a software configuration thing (in the kernel?)? If it is configurable, how do I make it work in 100Mbit/s mode? I have never heard of a Gigabit ethernet device not working with lesser speeds before. It seems like quite a limitation that would affect a number of people!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Thanks Gary. I hope to test the PetaLinux 2014.2 boot files soon.
    The funny thing is that I built my own Linux kernel using OpenEmbedded and the latest meta-xilinx layer: http://git.yoctoproject.org/cgit/cgit.cgi/meta-xilinx/. It has the same faulty Ethernet behaviour, which I thought was strange, as I would have expected it to be fixed in that repository.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Thanks Gary. I hope to test the PetaLinux 2014.2 boot files soon.
    The funny thing is that I built my own Linux kernel using OpenEmbedded and the latest meta-xilinx layer: http://git.yoctoproject.org/cgit/cgit.cgi/meta-xilinx/. It has the same faulty Ethernet behaviour, which I thought was strange, as I would have expected it to be fixed in that repository.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Sorry, that's not quite right. I switched to using the kernel from: https://github.com/Xilinx/linux-xlnx (because I couldn't get the PCIe slot working with OpenEmbedded). Which should still include all the latest fixes, so it's still strange the Ethernet isn't working there either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Hi,
    I just had the same Problem, and it is related to the Devicetree.
    Once I changed the values of the phy entry to the ones given in the
    2014.2 design it worked:
                                    phy0: phy@7 {
    -                                       compatible = "marvell,88e1116r";
    +                                       compatible = "marvell,88e1510";
                                            device_type = "ethernet-phy";
    -                                        reg = <7>;
    +                                        reg = <0>;
    +                                        marvell,reg-init=<3 16 0xff00 0x1e 3 17 0xfff0 0x0a>;
                                    } ;
                            } ;
    whether I should also change the phy@7 to a phy@0 I am currently investigating.