Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Mini-ITX Hardware Design Ethernet only working in Gigabit mode (not 100Mbit/s)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 343 subscribers
  • Views 754 views
  • Users 0 members are here
Related

Ethernet only working in Gigabit mode (not 100Mbit/s)

Former Member
Former Member over 11 years ago

I have a Gigabit ethernet card in my primary development computer. When I connect the Mini-ITX Zynq board directly to that (with static IPs on both), it works fine (testing with "ping <address>". However, if it connects through a 10/100Mbit/s switch, it fails to work. Similarly, another development computer with only a 10/100Mbit/s ethernet card directly connected does not work. This makes me conclude that ethernet in anything less than 1Gbit/s mode on the Mini-ITX does not work. I am using the stock standard microSD to boot up. I have also built up my own Linux kernel and image, which also has exactly the same issue.

I also have a Zedboard. With the stock standard SD to boot up, this does work in 100Mbit/s mode through the switch, and with the 100Mbit/s ethernet card in the development computer.

Is this a limitation of the hardware, or is it a software configuration thing (in the kernel?)? If it is configurable, how do I make it work in 100Mbit/s mode? I have never heard of a Gigabit ethernet device not working with lesser speeds before. It seems like quite a limitation that would affect a number of people!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    this setting will program PHY LEDs in DUAL LED MODE 3, with open drain outputs, is that what you intended todo?

    My guess is that the LEDS are not connected in dual mode on the ITX board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    this setting will program PHY LEDs in DUAL LED MODE 3, with open drain outputs, is that what you intended todo?

    My guess is that the LEDS are not connected in dual mode on the ITX board.