Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design IP Catalog with IP Integrator
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 935 views
  • Users 0 members are here
Related

IP Catalog with IP Integrator

e14 Contributor
e14 Contributor over 10 years ago

Hi

I have a Picozed Z030 and the FMC Carrier.  I want to implement Aurora 8b/10b on it.  I open the example, and I got all the vhdl files, but I donu00B4t know how to connect  the init_clk, drp_clk and the GT_REFCLK signals in the design.  How can I route the clocks from the zynq for connecting with the external signal required in the IP Catalog Aurora example.
I need 1 single clock for DRP_CLK and a differential clock for INIT_clk, both 50MHz and, 125MHZ for GT_REFCLK


 

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi abhaya,

    Have you taken a look at PG046 and XAPP1193 yet? 

    http://www.xilinx.com/support/documentation/ip_documentation/aurora_8b10b/v10_1/pg046-aurora-8b10b.pdf

    http://www.xilinx.com/support/documentation/application_notes/xapp1193-aurora-8b10b-on-kc705.pdf

    Although XAPP1193 is related to Kintex devices, most of the work for Aurora8b/10b is around the transceivers so most of the information should still be applicable.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thank you for the answer. I already look at that files, but   my problem is  how to define init_clk, drp_clk in my <file>.xdc using the picozed.  How do I get these signal from the PS ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi abhaya,


    Perhaps I am misunderstanding your question.

    If you are connecting those signals externally to the Zynq device, then look within your top level HDL for the port names and then you can use those port names for your XDC pin constraints.

    If you are connecting those signals directly to the Zynq Processing System, then you simply make the connection within the IP Integrator Block Design and then there is no need for an XDC pin constraint.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer