Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Picozed Power Enable
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 332 subscribers
  • Views 476 views
  • Users 0 members are here
Related

Picozed Power Enable

mugundhan
mugundhan over 7 years ago

Hello,

 

I'm designing a picozed carrier card. I'm a bit puzzled about the PWR_ENABLE input. In the FMC design, I see that the switch, when in off state supplies 12 V to the BSS138 (Q3) MOS, and the MOSFET is in open drain. It is said in documentation that till rev C there was an onboard pull up on the picozed itself, but it has been removed from the Rev E. Also, the data sheet of the TPS54618 says that the maximum value of power enable to the IC is only 4 V. So, i cannot follow connecting an external pull up to VIN_HDR, as was the case on previous versions of PicoZed (on board, till rev C) right ?

Secondly, can I connect it to the 3.3 V Power header ? Like 12V_OFF through a RC network for setting the time constant, and a pullup of 10k to 3.3V should be good to brnig up the power enable ?

 

Guidance would be appreciated ! :)