Hello,
I designed a custom carrier board for the PicoZed 7015/7030 and am trying to connect to its JTAG port using a JTAG-SMT2 USB to JTAG module. The problem is that it seems to recognize I'm connected to FPGA through the JTAG-SMT2 board, but I then get an error that states
"Could not find ARM device on the board for connection"
I have verified that my connection process is correct by successfully connecting to a ZedBoard via JTAG
Looking at the device manager, when I connect to the Zedboard, it shows up under 'Ports' as a USB Serial Port. However, when I connect to my custom carrier board/ PicoZed through the JTAG-SMT2, it doesn't show up under Ports, but rather just under Universal Serial Bus controllers as a 'USB Serial Converter'.
Is this a driver problem?