Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design SDcard not writeable on PicoZed Rev E board (Rev C board works) ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 340 subscribers
  • Views 1103 views
  • Users 0 members are here
Related

SDcard not writeable on PicoZed Rev E board (Rev C board works) ?

Former Member
Former Member over 7 years ago

We just got the first RevE 7020 module. With the RevC everything works.

We install the QSPI and eMMC through booting a small LINUX from SDcard.
With RevE the Linux boot stops with a Kernel panic or a maintenance request, when write access to the SD card is needed. It finds errors in the filesystem which are cleaned up with RevC. With RevE it just complains that no Write is possible and stops.

I tried to write something to the SDcard in UBOOT and that seems to work. Of course the SDcard is writeable in other computers.

 

Reinhard

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 7 years ago

    Hi Reinhard,

    Which Linux are you booting from the SD card?

    I am booting our PetaLinux 2017.4 image on Rev. E hardware without issues.  I am wondering if the write protect bit is not getting set properly within the devicetree and that is resulting in what you are seeing when moving from Rev. C to Rev. E?

    http://zedboard.org/content/emmc-not-found-picozed-rev-e-board-rev-c-board-works

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 7 years ago

    Hi Reinhard,

    Which Linux are you booting from the SD card?

    I am booting our PetaLinux 2017.4 image on Rev. E hardware without issues.  I am wondering if the write protect bit is not getting set properly within the devicetree and that is resulting in what you are seeing when moving from Rev. C to Rev. E?

    http://zedboard.org/content/emmc-not-found-picozed-rev-e-board-rev-c-board-works

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 7 years ago in reply to zedhed

    I'm booting Linux version 3.19.0-xilinx

    I tried the Pulsar Linux Image which works. But it uses another file system (btrfs). I tried the dtb entries from the Pulsar Image, but they differ too much from ours and only lead to other failures.

    Our dtb:

    ps7-sdio@e0100000 {
    clock-names = "clk_xin", "clk_ahb", "ref_clk", "aper_clk";
    clocks = <0x2 0x15 0x2 0x20 0x2 0x15 0x2 0x20>;
    clock-frequency = <0x2faf080>;
    compatible = "arasan,sdhci-8.9a", "arasan,sdhci", "generic-sdhci", "xlnx,ps7-sdio-1.00.a";
    interrupt-parent = <0x3>;
    interrupts = <0x0 0x18 0x4>;
    reg = <0xe0100000 0x1000>;
    xlnx,has-cd = <0x1>;
    xlnx,has-power = <0x0>;
    xlnx,has-wp = <0x0>;
    };


    ps7-sdio@e0101000 {
    clock-names = "clk_xin", "clk_ahb", "ref_clk", "aper_clk";
    clocks = <0x2 0x16 0x2 0x21 0x2 0x16 0x2 0x21>;
    clock-frequency = <0x1312d00>;
    compatible = "arasan,sdhci-8.9a", "arasan,sdhci", "generic-sdhci", "xlnx,ps7-sdio-1.00.a";
    interrupt-parent = <0x3>;
    interrupts = <0x0 0x2f 0x4>;
    reg = <0xe0101000 0x1000>;
    xlnx,has-cd = <0x1>;
    xlnx,has-power = <0x0>;
    xlnx,has-wp = <0x1>;
    non-removable;
    disable-hispd;
    };
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.