Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design SDcard not writeable on PicoZed Rev E board (Rev C board works) ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 340 subscribers
  • Views 1110 views
  • Users 0 members are here
Related

SDcard not writeable on PicoZed Rev E board (Rev C board works) ?

Former Member
Former Member over 7 years ago

We just got the first RevE 7020 module. With the RevC everything works.

We install the QSPI and eMMC through booting a small LINUX from SDcard.
With RevE the Linux boot stops with a Kernel panic or a maintenance request, when write access to the SD card is needed. It finds errors in the filesystem which are cleaned up with RevC. With RevE it just complains that no Write is possible and stops.

I tried to write something to the SDcard in UBOOT and that seems to work. Of course the SDcard is writeable in other computers.

 

Reinhard

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 7 years ago

    I found the reason for our problem. The FSBL was made by a third party. It uses 0 for the selection of WP (not used) to MIO0. That is OK for RevC, because it has jumper resistors, which give a stable voltage. The RevE has nothing connected to MIO0 and the floating(?) voltage is wrong. If I connect it to Gnd, it works.

    I still have to find out, why an image copy from SDcard to eMMC needs twice the time as before.

    Reinhard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 7 years ago

    I found the reason for our problem. The FSBL was made by a third party. It uses 0 for the selection of WP (not used) to MIO0. That is OK for RevC, because it has jumper resistors, which give a stable voltage. The RevE has nothing connected to MIO0 and the floating(?) voltage is wrong. If I connect it to Gnd, it works.

    I still have to find out, why an image copy from SDcard to eMMC needs twice the time as before.

    Reinhard
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.