Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio Software-Defined Radio with PicoZed™︎ SDR SpeedWay Workshop on-line / Model-based design flow from MathWorks
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 340 subscribers
  • Views 402 views
  • Users 0 members are here
Related

Software-Defined Radio with PicoZed™︎ SDR SpeedWay Workshop on-line / Model-based design flow from MathWorks

Former Member
Former Member over 9 years ago
 
  
   
    
     
       • Day 1 PM Lecture: Prototyping and testing with PicoZed SDR http://microzed.org/videos/prototyping-and-testing-picozed-sdr
     
        
     
       • Day 1 PM Lab: QPSK Receiver with Radio-in-the-Loop http://microzed.org/videos/qpsk-receiver-radio-loop
     
        
     
       In this lab we shall validate the QPSK receiver as a device under test (DUT), modeled within MATLAB and Simulink on the host PC, but with ‘live’ RF carrier-modulated traffic from the AD9361 as input stimulus. For a signal source, recorded QPSK baseband data will be stored in DDR3 memory of PicoZed SDR and repeatedly transmitted without gaps through the AD9361 RF front-end. This RF signal will be looped-back through the AD9361 RX to be digitized and sent over TCP/IP as I&Q baseband signals from PicoZed SDR to the QPSK receiver DUT running in Simulink on the PC. This methodology serves to validate the AD9361 front-end while allowing incremental refinements of the DUT model in the presence of ‘real-world’ signals.
     
        
     
       • Day 2 AM Lab: Integrating a QPSK Receiver into PicoZed SDR https://avnet.egnyte.com/dl/QYvqFX5vcT
     
        
     
       In this lab we shall optimize the QPSK receiver Simulink model for efficient hardware implementation, then build the entire system for stand-alone operation on PicoZed SDR. Using the automation within HDL Workflow Advisor from MathWorks, an IP core will be generated from the QPSK receiver model and integrated into a Vivado-based board support package custom-made for PicoZed SDR1. The design will be compiled to a bitstream and all necessary files will be created to boot PicoZed SDR for stand-alone operation.
     
        
     
       • Day 2 PM Lecture: Product Deployment with PicoZed SDR https://avnet.egnyte.com/dl/8PDE80mG7c
     
        
     
       From data stored in the filesystem of the SD card, a QPSK signal will be generated through the AD9361 DAC, sent over an RF carrier back to the AD9361 input and de-modulated by the QPSK receiver IP block in the Zynq device. Using PicoZed SDR as a single-board computer running Linux, the de-modulated QPSK will be displayed through the Analog Devices IIO Oscilloscope on an HDMI monitor and the payload logged to the serial console.
    
   
  
 
  Top 
    
 
     
  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 9 years ago

    The on-line videos of SDR SpeedWay lectures and labs are now posted on the main Avnet ‘Training & Events’ page https://products.avnet.com/wps/portal/ema/event/software-defined-radio-picozed-sdr-speedway-workshop-2015/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer