Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
RFSoC Boards Problems with the RFSoC Explorer and the resulting signal
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 357 subscribers
  • Views 1151 views
  • Users 0 members are here
  • bandwidth
  • zcu208
  • rfsoc explorer
  • matlab
  • Wireless Waveform Generator
Related

Problems with the RFSoC Explorer and the resulting signal

rcarli
rcarli over 1 year ago

Hey, 

I want to use the RFSoC to investigate the effect of different filters on the resulting analog signal. For this I use a DAC-ADC loop and an external signal analyzer. For this I use the RFSoc Explorer. This also works so far. However, I have the following problems:

When transferring the waveform from the Wireless Waveform Generator of Matlab, the following error message appears:

"Connected to RFTool
Board IP address 169.254.0.2
Error in executing callback registered with ViewModel:
Error using wwfg_callback
Unrecognized field name "pCurrentWaveformType"."

Is there a way to fix this?

The import from simulink does not work either. Here i get the message: "Unrecogized signal type"

Becouse of the error i exported the waveform as a Matlab script and generated the variable “Waveform.mat” with the complex data signal. According to the Matlab plot, this signal should have a bandwidth of about 1MHz. However, when I load the signal into the RFSoc Explorer and transfer it to the hardware, I get a bandwidth of approx. 40MHz. The same problem i get with my generated signals from Simulink, which I save as a complex data array as a .mat file.

The bandwidth should be similar to the simulated result, or am I forgetting something here? Is it possibly also due to the waveform read in?

My setup:

  • Xilinx ZCU208 RFSoC Gen 3
  • HW-XM655 Balun Card
  • Matlab 2023b
  • Avnet RFSoC Explorer 3.0.0 (with 3.1 i cant find the ZCU208 Board at the HDL Worklow Advisor)
  • "avnet_rfsocX_zcu208es1_boot_v1_1"- file
  • Keysight EXA Signal Analyzer 
{gallery}My Gallery Title

image

Settings RF Explorer

image

Settings for Simple Waveform to test

Thank you in advance and best regards

  • Sign in to reply
  • Cancel
Parents
  • LucLanglois
    0 LucLanglois over 1 year ago

    Thanks for reporting this issue.

    To aid debugging, may I ask you to share the resulting .MAT from WWFG-> 'Save Session' ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rcarli
    0 rcarli over 1 year ago in reply to LucLanglois

    Thank you for your quick feedback. I have now been able to solve the problem with the incorrect bandwidth myself. The generated waveform from the Matlab script was missing the correct time. After the Matlab 2023b update 8, I was at least able to import the directly exported Matlab file from the WWFG into the RFSoc Explorer. This was not possible before. With this file, I now get the expected spectrum.

    However, it is still not possible to import the waveform directly from the WWFG into the RF Explorer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rcarli
    0 rcarli over 1 year ago in reply to LucLanglois

    Thank you for your quick feedback. I have now been able to solve the problem with the incorrect bandwidth myself. The generated waveform from the Matlab script was missing the correct time. After the Matlab 2023b update 8, I was at least able to import the directly exported Matlab file from the WWFG into the RFSoc Explorer. This was not possible before. With this file, I now get the expected spectrum.

    However, it is still not possible to import the waveform directly from the WWFG into the RF Explorer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data