Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development More than one Zedboard in a Network
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 346 subscribers
  • Views 396 views
  • Users 0 members are here
Related

More than one Zedboard in a Network

eactor
eactor over 12 years ago

Right now I have 2 Zedboards connected to an Router. This led me to the problem that it can't distinguish between them? The both use the same mac adress  00:0A:35:00:01:22 to acquire a DHCP IP?
Where would I change the HW-Address of the Zedboard?
FSBL?
UBOOT?
Linux-KERNEL?
DEVICETREE?

Thanks

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 12 years ago

    setenv ethaddr 00:0a:35:00:01:23
    saveenv

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eactor
    0 eactor over 12 years ago in reply to Former Member

    On one of my Zedboards, the first command leads to an error:
    zed-boot> setenv ethaddr 00:0a:35:00:01:23
    Can't overwrite "ethaddr"

    On the other it does work, but how does the save work? It saves the Enviroment to SPI Flash? Even if I boot from SD card? What if my device doesn't have a QSPI or is that impossible?

    zynq-ubbot>saveenv
    SF: Detected S25FL256S with page size 64 KiB, total 32 MiB
    SF: Warning - Only lower 16MB is accessible in 3 byte addressing mode
    Erasing SPI flash...SF: Successfully erased 131072 bytes @ 0xe0000
    Writing to SPI flash...SF: program success 131072 bytes @ 0xe0000

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to eactor

    Probably the version/config is different. U-Boot has a feature to protect ethaddress and serial number that you can choose in config.

    U-boot stores its environment in the flash (QSPI on the Zedboard). You can also change the startup default in the sources, rebuild uboot and put it on the SD card.