Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Functioning project using Performance Monitor?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 190 views
  • Users 0 members are here
Related

Functioning project using Performance Monitor?

applefat
applefat over 11 years ago

Does anyone have a functioning reference design using the Xilinx Performance Monitor? I think my main problem might be the interconnects in XPS rather than the code.

My problem is the same as the one mentioned here, but I do not see any path issue as the OP found:

http://zedboard.org/content/using-xilin32-access-hardware-ip-registersaxiperfmon

Basically when I try to read back from the Perf. Monitor block (using Xil_In32 to read register 0x104 for instance, but also any other reg), the device hangs on the read. It's assigned 0x75C00000 and I just add the offset to get the absolute address. I can read/write successfully to my other peripherals in this way.

Xilinx has some examples using Vivado but there is no XPS project so I do not know how I can check the AXI interconnects (also the project versions are too new) ...


Update: Originally I was having slot 0 monitor an axilite bus going to one peripheral, and an axi bus going to another peripheral. But, both busses connect through the same axi_interconnect to M_AXI_GP0.  I deleted the AXI peripheral and reconfigured the performance monitor for one slot, and now I can read from the performance monitor. I'm not sure the correct way to configure the bus but at least I have a reference now.