Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development zedboard SDK load elf error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 349 subscribers
  • Views 748 views
  • Users 0 members are here
Related

zedboard SDK load elf error

Former Member
Former Member over 9 years ago

zedboard hardware project use vivado 2014.4 embedded zedboard zynq evaluation and development kit design without any modification.Generate bitstream directly and program device successfully.
Then i lanuch SDK and use helloworld application without any modification.after i build it and run error occured:

problem occured window :
An internal error occurred during: "Launching New_configuration".
No Target with ID 64 in the System

SDK log:
21:37:04 INFOt: Processor reset is completed for ps7_cortexa9_0
21:37:07 ERRORt: Unexpected error while launching program.
java.lang.RuntimeException: Failed to download ELF file


    AP transaction error (DP CTRL_STAT=0xf0000021)
    Error Address = 0x00100000, Size = 0x00000004


tat com.xilinx.sdk.targetmanager.internal.TM.downloadELF(TM.java:666)
tat com.xilinx.sdk.debug.core.internal.AppRunner.run(AppRunner.java:129)
tat com.xilinx.sdk.debug.core.XilinxAppLaunchConfigurationDelegate.runApplication(XilinxAppLaunchConfigurationDelegate.java:605)

at the beginning i used this process run helloworld application can read helloworld at serial port.but these days error occurred. who knows what is the problem?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 9 years ago

    I'm not sure about this answer but you could check into it.

    I find it suspicious that the error address is 0x100000.  This is the beginning of the DDR memory.  You could be trying to write the program to 0x100000 and then run it from there too (overwriting something).  Try going into the linker script and running the program from the OCM RAM instead of the DDR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    I'm not sure about this answer but you could check into it.

    I find it suspicious that the error address is 0x100000.  This is the beginning of the DDR memory.  You could be trying to write the program to 0x100000 and then run it from there too (overwriting something).  Try going into the linker script and running the program from the OCM RAM instead of the DDR.