Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Program flash memory without Xilinx platform cable
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 343 subscribers
  • Views 323 views
  • Users 0 members are here
Related

Program flash memory without Xilinx platform cable

Former Member
Former Member over 9 years ago

I am using a picozed board with the Zynq 7015 processor. I can currently generate either a *.mcs or *.bin image and boot either from the QSPI memory or a SD card. In the field, I would prefer not to have any platform cable connected. The SD card option would be interesting, but since the board will be moving at high speed, I am afraid it is not a viable option. My question is: is it possible to write to the flash memory without being connected with the platform cable? Like sending the file through serial port (preferred option), or reading it from the SD card (removed after)? By the way, the application uses the standalone OS.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 9 years ago

    Melanie,

    Yes, you can definitely read/write QSPI from a standalone software program.  U-boot, for example, has commands to do just that.  There are a variety of means available for obtaining the data, which could be via ethernet, SD card or serial (not sure if that last one is standard off the top of my head, but reading from serial is not difficult - there are plenty of standalone examples).  Or you can just look at how U-boot does the programming and incorporate the open source into your own program (with the appropriate GNU disclaimers).

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    Melanie,

    Yes, you can definitely read/write QSPI from a standalone software program.  U-boot, for example, has commands to do just that.  There are a variety of means available for obtaining the data, which could be via ethernet, SD card or serial (not sure if that last one is standard off the top of my head, but reading from serial is not difficult - there are plenty of standalone examples).  Or you can just look at how U-boot does the programming and incorporate the open source into your own program (with the appropriate GNU disclaimers).

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.