Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Updated Open Source Linux Ethernet Performance Test Tutorial Posted
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 337 subscribers
  • Views 406 views
  • Users 0 members are here
Related

Updated Open Source Linux Ethernet Performance Test Tutorial Posted

zedhed
zedhed over 10 years ago

Hello,

 

I just wanted to let everyone know that the Open Source Linux Ethernet Performance Tutorial has been migrated to Vivado 2014.4 and updated for ZedBoard, MicroZed, and added support for PicoZed.  We also added some different tests into the performance report in case you are looking for an idea on what numbers to expect in your own test experiments.

 

These updated Reference Designs/Tutorials can be downloaded from our community sites using a registered login which is available free of charge to anyone:

 

Fullscreen contentimage_53553.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

ZedBoard:

 

http://zedboard.org/support/design/1521/11

 

MicroZed:

 

http://microzed.org/support/design/1519/10

 

PicoZed:

 

http://picozed.org/support/design/4736/71

 

There have been quite a few changes over previous (ISE based) versions with this latest update.  Using one of the later kernel tags is definitely helping performance numbers and by switching to a Linux PC that helps the numbers even more.  On tests run using a 2014.4 tagged kernel and a CentOS 7 test laptop, we are seeing throughput rates as high ~800 Mbps reported by iperf3 which is significant improvement over earlier iterations. 

 

Fullscreen contentimage_53554.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

Please keep in mind that results will vary based upon varying network configuration and tuning parameters.  Hopefully you can find this information useful for evaluaing our Zynq boards.

 

Regards,

 

-Kevin

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Also discovered something from another user following these instructions but building on an Ubuntu 12.04 host machine rather than CentOS.

    -------------------------------------------------

    The following error was observed when iperf3 was launched on the Ubuntu host:

    architech@architech:~$ iperf3
    iperf3: error while loading shared libraries: libiperf.so.0: cannot open shared object file: No such file or directory

    -------------------------------------------------

    After building iperf3 under Ubuntu and running 'make install' the shared library cache does not appear to get updated automatically like it does under CentOS.

    I think you have two options once you get to this point:
    1)tReboot the host machine
    2)tRun u201Csudo ldconfigu201D to force the shared library cache to get updated with the latest libraries found in /lib and /usr/lib (which should now include libiperf.so.0)

    Hopefully this is helpful for anyone going through these tutorials under Ubuntu.

    Regards,

    -Kevin