Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development [Solved] unrecognized/unsupported machine ID@Ubuntu Desktop Linux in Reference Designs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 1865 views
  • Users 0 members are here
Related

[Solved] unrecognized/unsupported machine ID@Ubuntu Desktop Linux in Reference Designs

Former Member
Former Member over 13 years ago

hello
after I was doing Reference Designs-linaro ubuntu desktop step by step, I insert the SD card into zedboard and power on.

but it boot error,
here is the UART info
#####################################################
Welcome to minicom 2.6

OPTIONS: I18n
Compiled on Apr 13 2013, 09:38:52.
Port /dev/ttyACM0

Press CTRL-A Z for help on special keys



U-Boot 2011.03 (May 08 2013 - 16:28:01)

DRAM:  512 MiB
MMC:   SDHCI: 0
Using default environment

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI                                                                  
Manufacturer ID: 12                                                            
OEM: 3456                                                                      
Name: SMI                                                                      
Tran Speed: 25000000                                                           
Rd Block Len: 512                                                              
SD version 1.10                                                                
High Capacity: Yes                                                             
Capacity: 3967811584                                                           
Bus Width: 1-bit                                                               
reading zImage

2816560 bytes read                                                          

reading devicetree.dtb                                                

8282 bytes read                                                                
reading ramdisk8M.image.gz                                            ttttttt3694108 bytes read                                                           
## Starting application at 0x00008000 ...                                      
tttttttUncompressing Linux... done, booting the kernel.                              
ttttttt
Error: unrecognized/unsupported machine ID (r1=0x1fb71dd0).                  
ttttttttttttttAvailable machine support:                                                     
ID (hex)       NAME                                                       ttttttt00000d32        Xilinx Zynq Platform                                          
t
Please check your kernel config and/or bootloader.
########################################################

why did the error happen?

what's wrong with the boot.bin or zImage or devicetree.dtb?

I just do step by step as the pdf says

  • Sign in to reply
  • Cancel
Parents
  • joswa
    0 joswa over 12 years ago

    I've the same problem but can't find any solution. Any one pls. help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • joswa
    0 joswa over 12 years ago

    I've the same problem but can't find any solution. Any one pls. help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to joswa

    I have solved it.
    see
    http://ez.analog.com/message/87877
    in linux kernel config
    set
    CONFIG_XILINX_FIXED_DEVTREE_ADDR=y
    it works for me

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer