element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design I/O voltage pins on Ultra96-V2 for CANBUS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 318 subscribers
  • Views 743 views
  • Users 0 members are here
  • io voltage
  • canbus
Related

I/O voltage pins on Ultra96-V2 for CANBUS

nico_n04
nico_n04 over 5 years ago

I saw that the header expansion uses 1.8V.  I have added canbus support to the slow speed expansion header (J7).

the slave devices I am using on the buses uses 3.3 Volts , I saw on a forum that I can use a level shift but  I would rather use 3.3 Volts directly from the board.

 

Is the way to configure the board to use 3.3 Volts for the VCC_PAUX from the schematics?

I would assume the high speed expansion header also uses 1.8 V as well? is there a set of pins from one of the banks set to use 3.3 Volts?

  • Sign in to reply
  • Cancel

Top Replies

  • nico_n04
    nico_n04 over 5 years ago +1 suggested
    Found the answer on the Hardware user Guide: 5.1.2 Zynq UltraScale+ MPSoC Promammable Logic (PL) provides two types of I/O banks: High-density (HD) banks and high-performance (HP) banks. HD banks support…
  • bhfletcher
    bhfletcher over 5 years ago in reply to nico_n04 +1
    The recently released Click Mezzanine for Ultra96 already has the level shifters built in. It makes for very quick and easy prototyping. You can see more about the mezzanine here: 96Boards Click Mezzanine…
  • nico_n04
    0 nico_n04 over 5 years ago

    Found the answer on the Hardware user Guide: 5.1.2

    Zynq UltraScale+ MPSoC Promammable Logic (PL) provides two types of I/O banks: High-density (HD) banks and high-performance (HP) banks. HD banks support a limited number of single-ended I/O standards with speeds up to 250Mbps and VCCO voltages up to 3.30V. HP banks support a large variety of high-speed I/O standards, including differential I/O, and support VCCO voltages up to 1.80V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nico_n04
    0 nico_n04 over 5 years ago in reply to nico_n04

    I like to add that HP and HD banks are on the PL side so they are can not be configured to use for the can bus from the PS. So I would need to use the logic level shifter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 5 years ago in reply to nico_n04

    The recently released Click Mezzanine for Ultra96 already has the level shifters built in. It makes for very quick and easy prototyping. You can see more about the mezzanine here:

    96Boards Click Mezzanine | Zedboard

     

    You will also find 10 different CAN Click boards available. Note, I have not used any of them, and I'm not aware of anyone using them yet. If you are successful, please share with the community!

    https://www.mikroe.com/click?type*=can,can

     

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.