Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design ON Semiconductor Dual Camera Mezzanine Support
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • +1 person also asked this people also asked this
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 347 subscribers
  • Views 2021 views
  • Users 0 members are here
  • ultra96
  • pynq
  • 96boards on semiconductor dual camera mezzanine
Related

ON Semiconductor Dual Camera Mezzanine Support

cstarr
cstarr over 4 years ago

Hi,

 

Does anyone know where I can find driver information for the ON Semi Mezzanine board?

 

So far, I have followed the "Getting Started" document, running the Petalinux image and starting a preinstalled program that shows the camera feed on a monitor. I am unsure where to go from there. Eventaully, I would like to use PYNQ, but do not see any documention on how to install the driver.

  • Sign in to reply
  • Cancel

Top Replies

  • ctammann
    ctammann over 4 years ago +2 suggested
    Hey everyone, I just wanted to chime in so you knew I was working on this request. We currently don't have a stand alone driver, although we are working towards releasing one. That will be a while though…
  • jomoenginer
    jomoenginer over 4 years ago +1 suggested
    What sort of driver are you looking for? Adam Taylor at Hackster.io has a pretty good example of building a Vivado project for the Ultra96 and the Dual Camera Mezzanine. https://www.hackster.io/adam-taylor…
  • jomoenginer
    jomoenginer over 4 years ago in reply to cstarr +1
    This interests me as well considering I am currently working on a RoadTest for the Ultra96 and the Dual Camera Mezzanine. From what I can tell, there is little in the way of examples and such for the 96Boards…
  • jomoenginer
    0 jomoenginer over 4 years ago

    What sort of driver are you looking for?

     

    Adam Taylor at Hackster.io has a pretty good example of building a Vivado project for the Ultra96 and the Dual Camera Mezzanine.

    https://www.hackster.io/adam-taylor/avnet-ultra96-and-onsemi-dual-mipi-camera-3492ab

     

    He does mentioning attempting moving to PYNQ with the Ultra96 and the Dual Camera Mezzanine, but I am not sure if he has completed this.

    You might start here but I do not see anything specific with regards to the Dual Camera board though:

    https://github.com/Avnet/Ultra96-PYNQ

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cstarr
    0 cstarr over 4 years ago in reply to jomoenginer

    Thanks for the reply!

     

    I am new the Ultra96 and Xilinx, and was hoping to avoid using Vivado. It seems like there is a bit of a learning curve, and PYNQ is pretty user friendly and has everything I need on it aside from a driver for the Dual Cam Mezzanine board.

     

    As far as what type of driver, I am looking for a Linux driver so I can access the camera from a python script - specifically using openCV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 4 years ago in reply to cstarr

    This interests me as well considering I am currently working on a RoadTest for the Ultra96 and the Dual Camera Mezzanine.

     

    From what I can tell, there is little in the way of examples and such for the 96Boards ON Semiconductor Dual Camera Mezzanine and nothing I could find with regards to PYNQ.

     

    There is this post on element14 with regards to building a PetaLinux image for the Ultra96 V2 and Dual Camera Mezzanine but nothing specific to OpenCV or PYNQ again:

    https://www.element14.com/community/groups/fpga-group/blog/2021/01/14/ultra96-v2-dual-camera-mezzanine-petalinux-build-instructions

     

    You could try to start with an example using the Ultra96-V2 and Python and see if you can add the Dual Camera Mezzanine instead of the USB camera.

    Ex:

    https://www.hackster.io/AlbertaBeef/face-detection-and-tracking-in-python-on-ultra96-v2-02d104

     

     

    If I come up with something, I'll post it.

     

    Cheers,

     

    Jon

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 4 years ago

    Hey everyone,

     

    I just wanted to chime in so you knew I was working on this request. We currently don't have a stand alone driver, although we are working towards releasing one. That will be a while though so I'm trying to figure something else out. We haven't done any development with this platform using PYNQ so unfortunately I do not have any reference designs to share. I'll post back with anything I'm able to come up with ASAP.

    Thanks
    Chris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cstarr
    0 cstarr over 4 years ago in reply to ctammann

    Thanks for the info, Chris.

     

    For now, I want to just capture an image from the Mezzanine board using the petalinux image. I see there is some kind of driver available because the device registers under "/dev/media*" and "dev/video*", and the "run_1920_1080" script of course streams this video. Interestingly, any attempt to capture this image using openCV in python fails (it us successful with other basic UVC compliant webcams).

     

    Am I meant to be able to do anything with the petalinux image that ships with the Mezzanine board aside from running the "run_1920_1080" program?

     

    Thanks,

    Chelsea

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 4 years ago in reply to cstarr

    Chelsea,

     

    What is the error that you are seeing when using OpenCV?

     

    Looking at the "run_1920_1080" script, it appears it is setting up the two Cameras  via meida-ctl and then uses the /dev/video0 device to capture an image.  I wonder if you need to set-up the two cameras first before using them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 4 years ago in reply to jomoenginer

    With regards to PYNQ support with the Ultra96 and the Dual Camera Mezz, perhaps the PYNQ Computer Vision code would be a place to start:

    https://github.com/Xilinx/PYNQ-ComputerVision

    https://github.com/Xilinx/PYNQ-ComputerVision/blob/master/overlays/README.md

     

    This would require some work though considering the base branch is 2 years old..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstarr
    0 cstarr over 4 years ago in reply to jomoenginer

    Hi Jon,

     

    I don't actually get an error, OpenCV just captures an empty image (filesize is 0).

     

    I think you are right in that I am not setting something up correctly.

     

    I had made a silly assumption that the "run_1920_1080" program was only available as a binary, as it was in the bin folder! Your posted prompted me to take a second look. I think this tells me enough on how to interact with the driver to move forward.

     

    Thank you!
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.