element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96-V2 No Wifi or Bluetooth
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • +1 person also asked this people also asked this
  • Replies 9 replies
  • Subscribers 317 subscribers
  • Views 2113 views
  • Users 0 members are here
  • ultra96v2
  • bluetooth
  • ultra96-v2
  • wifi
  • wilc3000
  • ultra96
Related

Ultra96-V2 No Wifi or Bluetooth

redmed
redmed over 1 year ago

Hello everyone,

I have recently bought an Ultra96 V2. I managed to flash the SD card with the latest OOB image available from Avnet but the Ultra96 doesn't bring up the Access Point and it doesn't work either when I try with the ./wifi.sh script.
I also tried with the latest Pynq image and I also built with petalinux the latest U96V2 SBC BSP (2022.2) but nothing changes.

Here is the error I have at boot time:

[   13.881500] wilc_sdio mmc1:0001:1 p2p0: Failed to get RSSI value
[   13.894769] power up request for already powered up source Wifi
[   13.900811] wilc_sdio mmc1:0001:1 p2p0: Failed to set driver handler
[   13.907269] wilc_sdio mmc1:0001:1 p2p0: Failed to get mac address
[FAILED] Failed to start Access point for Ultra96.

When trying with wifi.sh:

root@u96v2-sbc-base-2022-2:~# ./wifi.sh
Stopping Connection Manager
ifdown: interface wlan0 not configured
Successfully initialized wpa_supplicant
nl80211: kernel reports: Authentication algorithm number required[  442.409487] power up request for already powered up source Wifi
[  443.164679] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED
Could not set interface wlan0 flags (UP): Timer expired
nl80211:[  443.171509] wilc_sdio mmc1:0001:1 wlan0: Failed to frame register
 Could not set interface 'wlan0' UP
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
wlan0: Failed to initialize driver interface
[  443.201258] power up request for already powered up source Wifi
[  443.207246] wilc_sdio mmc1:0001:1 wlan0: Failed to set driver handler
[  443.213759] wilc_sdio mmc1:0001:1 wlan0: Failed to get mac address
RTNETLINK answers: Invalid argument
udhcpc: started, v1.34.1
[  444.653053] power up request for already powered up source Wifi
[  445.404683] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED
RTNETLINK answers: Timer expired
udhcpc: broadcasting discover
udhcpc: sendto: Network is down
udhcpc: read error: Network is down, reopening socket

And finally the errors I've got when trying to bring up the Bluetooth interface:

root@u96v2-sbc-base-2022-2:~# ./bt.sh
[  470.128734] wilc_sdio mmc1:0001:1 wlan0: Failed to set driver handler
[  470.156962] wilc_sdio mmc1:0001:1 p2p0: Failed to set driver handler
[  472.365450] wilc_sdio mmc1:0001:1 wlan0: Failed to get RSSI value
Device setup complete
[  475.644614] Bluetooth: hci0: command 0x1003 tx timeout
[  477.660590] Bluetooth: hci0: command 0x1001 tx timeout
[  479.676581] Bluetooth: hci0: command 0x1009 tx timeout
[  479.681822] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED

I could access another Ultra96 V2 and with the same OOB, the Wifi was brought up so I thought it was an hardware issue with my board. But when I got my new Ultra96 V2 board (100% sure that it's NOT the same as the 1st one), I've got the same issue.

Is there anything special to do or change to use the Wifi/BT module?

Thank you very much.

  • Sign in to reply
  • Cancel

Top Replies

  • redmed
    redmed over 1 year ago in reply to embeddedguy +1
    No, indeed, it doesn't appear in the output of ifconfig: root@u96v2-sbc-base-2022-2:~# ip a s 1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000 link/loopback…
Parents
  • embeddedguy
    0 embeddedguy over 1 year ago

    Hi,

    It could be hard to find out the right issue with Bluetooth and WiFi and why it's not working but therre are some standard Linux commands which could help.

    From above logs, it seems that wifi interface is not up.

    ifdown: interface wlan0 not configured

    You can try something like

    $sudo ifconfig interfacename up

    then for bluetooth

    $sudo bluetoothctl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • redmed
    0 redmed over 1 year ago in reply to embeddedguy

    Thank you for your reply.

    Unfortunately, it gives me an error too:

    root@u96v2-sbc-base-2022-2:~# ifconfig wlan0 up
    [   73.930335] power up request for already powered up source Wifi
    [   74.688702] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED
    ifconfig: SIOCSIFFLAGS: Timer expired

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • embeddedguy
    0 embeddedguy over 1 year ago in reply to redmed

    That looks scary to me. I checked on internet and this error can be if network interface is damaged. What is the output of ifconfig? do you see wifi device?

    Or try similar command which lists system hardware.

    • To avoid breaking the devices, do double-check that the interface is down whenever you want to change the connection. A broken NIC port will result in the ‘ifconfig: SIOCSIFFLAGS: Timer expired’ error when initiating the interface.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • redmed
    0 redmed over 1 year ago in reply to embeddedguy

    No, indeed, it doesn't appear in the output of ifconfig:

    root@u96v2-sbc-base-2022-2:~# ip a s
    1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
        link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
        inet 127.0.0.1/8 scope host lo
           valid_lft forever preferred_lft forever
        inet6 ::1/128 scope host 
           valid_lft forever preferred_lft forever
    2: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN group default qlen 1000
        link/sit 0.0.0.0 brd 0.0.0.0
    3: wlan0: <BROADCAST,MULTICAST> mtu 1500 qdisc noop state DOWN group default qlen 1000
        link/ether 00:00:00:00:00:00 brd ff:ff:ff:ff:ff:ff
    4: p2p0: <BROADCAST,MULTICAST> mtu 1500 qdisc noop state DOWN group default qlen 1000
        link/ether 00:00:00:00:00:00 brd ff:ff:ff:ff:ff:ff
    root@u96v2-sbc-base-2022-2:~# ifconfig
    lo        Link encap:Local Loopback  
              inet addr:127.0.0.1  Mask:255.0.0.0
              inet6 addr: ::1/128 Scope:Host
              UP LOOPBACK RUNNING  MTU:65536  Metric:1
              RX packets:152 errors:0 dropped:0 overruns:0 frame:0
              TX packets:152 errors:0 dropped:0 overruns:0 carrier:0
              collisions:0 txqueuelen:1000 
              RX bytes:12280 (11.9 KiB)  TX bytes:12280 (11.9 KiB)

    As you can see, it's state is "DOWN" in the ip command output...

    So it seems that I was unlucky and got 2 bad boards in a row.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • redmed
    0 redmed over 1 year ago in reply to embeddedguy

    I was looking at the board and I am not sure but some pins don't seem to be well soldered (right above the blue buttons)? I will take a look at the board I know works correctly and will compare just to be sure...

    From the datasheet, they are not the Not Connected pins: ww1.microchip.com/.../70005327A.pdf
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • embeddedguy
    0 embeddedguy over 1 year ago in reply to redmed

    Perhaps check with multimeter for continuty and the pins which are supposed to be connected are connected well..And check this onto the board which is working correctly. compare the results.

    If you can not exchange the board(I assume that boards from Avnet do not come with garranty/warranty etc), then try to solder the pins yourself.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • misaz
    0 misaz over 1 year ago in reply to embeddedguy

    Continuity test can be dangerous in this situation: https://electronics.stackexchange.com/questions/56066/continuity-tests-risks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • misaz
    0 misaz over 1 year ago in reply to embeddedguy

    Continuity test can be dangerous in this situation: https://electronics.stackexchange.com/questions/56066/continuity-tests-risks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.