element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultra96 Hardware Design Ultra96-V2 No Wifi or Bluetooth
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • +1 person also asked this people also asked this
  • Replies 9 replies
  • Subscribers 312 subscribers
  • Views 2095 views
  • Users 0 members are here
  • ultra96v2
  • bluetooth
  • ultra96-v2
  • wifi
  • wilc3000
  • ultra96
Related

Ultra96-V2 No Wifi or Bluetooth

redmed
redmed over 1 year ago

Hello everyone,

I have recently bought an Ultra96 V2. I managed to flash the SD card with the latest OOB image available from Avnet but the Ultra96 doesn't bring up the Access Point and it doesn't work either when I try with the ./wifi.sh script.
I also tried with the latest Pynq image and I also built with petalinux the latest U96V2 SBC BSP (2022.2) but nothing changes.

Here is the error I have at boot time:

[   13.881500] wilc_sdio mmc1:0001:1 p2p0: Failed to get RSSI value
[   13.894769] power up request for already powered up source Wifi
[   13.900811] wilc_sdio mmc1:0001:1 p2p0: Failed to set driver handler
[   13.907269] wilc_sdio mmc1:0001:1 p2p0: Failed to get mac address
[FAILED] Failed to start Access point for Ultra96.

When trying with wifi.sh:

root@u96v2-sbc-base-2022-2:~# ./wifi.sh
Stopping Connection Manager
ifdown: interface wlan0 not configured
Successfully initialized wpa_supplicant
nl80211: kernel reports: Authentication algorithm number required[  442.409487] power up request for already powered up source Wifi
[  443.164679] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED
Could not set interface wlan0 flags (UP): Timer expired
nl80211:[  443.171509] wilc_sdio mmc1:0001:1 wlan0: Failed to frame register
 Could not set interface 'wlan0' UP
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
wlan0: Failed to initialize driver interface
[  443.201258] power up request for already powered up source Wifi
[  443.207246] wilc_sdio mmc1:0001:1 wlan0: Failed to set driver handler
[  443.213759] wilc_sdio mmc1:0001:1 wlan0: Failed to get mac address
RTNETLINK answers: Invalid argument
udhcpc: started, v1.34.1
[  444.653053] power up request for already powered up source Wifi
[  445.404683] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED
RTNETLINK answers: Timer expired
udhcpc: broadcasting discover
udhcpc: sendto: Network is down
udhcpc: read error: Network is down, reopening socket

And finally the errors I've got when trying to bring up the Bluetooth interface:

root@u96v2-sbc-base-2022-2:~# ./bt.sh
[  470.128734] wilc_sdio mmc1:0001:1 wlan0: Failed to set driver handler
[  470.156962] wilc_sdio mmc1:0001:1 p2p0: Failed to set driver handler
[  472.365450] wilc_sdio mmc1:0001:1 wlan0: Failed to get RSSI value
Device setup complete
[  475.644614] Bluetooth: hci0: command 0x1003 tx timeout
[  477.660590] Bluetooth: hci0: command 0x1001 tx timeout
[  479.676581] Bluetooth: hci0: command 0x1009 tx timeout
[  479.681822] wilc_sdio mmc1:0001:1 wlan0: WLAN initialization FAILED

I could access another Ultra96 V2 and with the same OOB, the Wifi was brought up so I thought it was an hardware issue with my board. But when I got my new Ultra96 V2 board (100% sure that it's NOT the same as the 1st one), I've got the same issue.

Is there anything special to do or change to use the Wifi/BT module?

Thank you very much.

  • Sign in to reply
  • Cancel

Top Replies

  • redmed
    redmed over 1 year ago in reply to embeddedguy +1
    No, indeed, it doesn't appear in the output of ifconfig: root@u96v2-sbc-base-2022-2:~# ip a s 1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000 link/loopback…
Parents
  • lightcollector
    0 lightcollector over 1 year ago

    Hi,  Circumstantially it does seem like a hardware issue, may be a bad batch (purely speculation at this point).  If it helps any, the PYNQ image for V2 has a Jupyter Notebook that can be used to connect to a wifi AP.  If the interface isn't present the NB will probably fail with some cryptic messages, there are some startup scripts that invoke the driver and setup the user space access.  The PYNQ wifi module scripts can be found here: https://github.com/Avnet/Ultra96-PYNQ/tree/master/Ultra96/packages/wilc3000

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • lightcollector
    0 lightcollector over 1 year ago

    Hi,  Circumstantially it does seem like a hardware issue, may be a bad batch (purely speculation at this point).  If it helps any, the PYNQ image for V2 has a Jupyter Notebook that can be used to connect to a wifi AP.  If the interface isn't present the NB will probably fail with some cryptic messages, there are some startup scripts that invoke the driver and setup the user space access.  The PYNQ wifi module scripts can be found here: https://github.com/Avnet/Ultra96-PYNQ/tree/master/Ultra96/packages/wilc3000

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.