I have a black SOM and carrier card of Ultrazed from which I assume that I have the production SOM. This meant that I did not have to add an init.tcl file in the scripts folder for adding the board definition files. But the ultrazed board option became available in Vivado only after I added the tcl file in the scripts folder.
I have followed the UltraZed-EG Starter Kit Tutorial for vivado 2016.4 but I am working with 2017.4. I am unable to run a hello world application from Xilinx SDK on the Ultrazed board. If gives the following error: