Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Error Scanning JTAG Chain
  • Forums
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Avnet Boards Forums requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 46 subscribers
  • Views 816 views
  • Users 0 members are here
Related

Error Scanning JTAG Chain

Former Member
Former Member over 9 years ago

If I connect the Zedboard via JTAG I get the following error in XMD:

XMD% connect arm hw
Error:No devices detected while scanning the JTAG chain
ERROR: Failed to Scan JTAG Chain
        Unknown Error

I followed the instructions in:

ZedBoard Configuration and Booting Guide V 1.1 Aug 2012

setting all the MIO jumpers to ground.

I have also tried a Xlinx PLatform Cable and get the same error.

I am running Xilinx 14.3 (Windows 7/64) which works with an ML507 board. The board's JTAG device is installed (Driver: FTDI v2.8.24.0) and this is detected by Adept as device "Zed":

===== Digilent Adept  Rev 2.2.0 =====
Loading board information...
Warning:  Could not find specific board information
Initializing Scan Chain...
Default information loaded.
Initialization Complete.
It then says "No Devices identified"

This would suggest both JTAG programmers and software are working, but the problem is on the board with the JTAG chain. Please help. Thanks.

  • Reply
  • Cancel
  • Cancel
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi bkeitch,

    After looking at this a little bit closer, I think I understand what is going on here.  The ZedBoard JTAG chain was designed to allow the FMC JTAG chain to be inserted into the scan chain which would allow for things like Boundary Scan Test or In-Circuit Programming of FMC devices.  When an FMC is attached to ZedBoard, the Carrier (in this case ZedBoard) FMC present signal FMC-PRSNT gets pulled down by the module.  This in turn enables the buffers in IC1 to connect the ZedBoard JTAG signals to their FMX-x equivalents.  Likewise, IC2 is a selector IC which connects the TDI-USB signal to FMC-TDO instead of the default TDO-FPGA signal.  

    So unless the chain gets completed on the FMC by connecting additional IC JTAG TAPs, when an FMC is connected, there is no longer a solid path for TDO-FPGA to reach the ZedBoard J15 connector OR the USB-JTAG circuit.  This would explain why you see interference with the Platform Cable when connecting your FMC-XM105 card.

    On some of the FMC cards, there is a series resistor before FMC-PRSNT reaches GND which would give one option for disabling FMC-PRSNT and restoring the chain.  However, that is not the case with the FMC-XM105 since FMC-PRSNT is tied directly to GND. 

    Looking closer, it does appear that the FMC JTAG signals reach the J5 connector on FMC-XM105.  I do not have an FMC-XM105 to try this on here, but it seems like you should be able to put a jumper across pins 6 and 7 on J5 and restore a signal path to the Carrier board to complete the JTAG chain.

    That might not be the ultimate solution, but I don’t think that you would damage anything by trying this either.  If it does solve the problem, could you please let us know?

     

    Regards,

    -Kevin

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to zedhed

    Kevin,

    Thanks so much for explaining that and taking the time to look into it. Yes, the jumped does work. I think this will be useful for everyone using the FMC-105 board with the Zedboard.

    Ben

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to zedhed

    Kevin,

    Thanks so much for explaining that and taking the time to look into it. Yes, the jumped does work. I think this will be useful for everyone using the FMC-105 board with the Zedboard.

    Ben

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
Children
No Data