Hi Rathseg,
I am going to suggest that you go through the tutorial using Vivado/SDK 2014.2. The reason for this is that as Vivado releases updates, the various IPs, Drivers, design Flow tends to change/tweak a bit. For instance you noticed one difference yourself as you asked about the generate block design pop up window(default selection should be fine.).
So please run through the tutorial using the 2014.2 tool version and report back if this solved your issue.
--Josh
Yeah, that solved it. Thanks.
Given how basic that tutorial was though, does that mean that the zedboard is not really supported on anything other than 2014.2? Should I only use 2014.2 for all my work with the zedboard? The differences between 2014.2 and 2016.4 seemed to be small user interface differences, not much of substance, so unless a behind the scenes default setting/value got changed it seems like it should have still worked. I went through all the Release notes for the versions after 2014.2 and it looks like there are a fair bit of performance improvements to Vivado, which while not essential would be nice to have.
Hi Rathseg,
We always suggest to use the newest version of Vivado when doing your own/new development. The Zedboard and all of our Zynq producs are most defeinitly supported in Vivado 2016.4. Like I said in the previous post, your issue most likely stems from a driver/IP update. If you look at the change log of various IPs/Drivers you used I am sure there were some significant changes in the last two years(2014.2 was release about 2 years ago).
--Josh