Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Using Xilinx Tools Forum Error building OOB Design in ISE 14.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Avnet Boards Forums requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 109 subscribers
  • Views 383 views
  • Users 0 members are here
  • ise
  • vivado
  • xilinx vivado for linux
  • linux
Related

Error building OOB Design in ISE 14.4

bent9
bent9 over 4 years ago

Hi

I am trying to build the out-of-box design myself, so I can modify it.

I tried to follow this guide, but cannot generate the bitstream using xilinx platform studio that came with ISE 14.4 (The version that was used in the guide). I get the following Error when generating the bitstream the Design, without making any changes:

 

Failed to run core generator for <system_axi_interconnect_2_wrapper_fifo_generator_v9_1_1> macro.

 

I cannot figure out why. Does anybody have an Idea what to do?

 

I would much rather use Vivado 2018.3, has somebody ported the out-of-box project so that it can be built with Vivado?

I am very inexperienced with Vivado as well, is there any easy way to replicate the project so I can use it with the digilent linux kernel?

Thank you!

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 4 years ago

    Hello Be Tut,

     

    That is a Digilent reference design, thus I would suggest you ask this question over on their forum.

    They should know if it has been ported to the latest Vivado 2018.3.


    Thanks!

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bent9
    0 bent9 over 4 years ago in reply to jafoste4

    Hi Josh,

    seems like a better place to ask such a question, thanks for the pointer!

    If anybody stumbles across this post because of a similar issue, the thread I just created in the digilent forum can be found here.

    If there is a valid solution, I will make sure to update this thread to reflect it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
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
An Avnet Company © 2023 Premier Farnell Limited. All Rights Reserved.