Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AXI_MASTER_BURST 256bits IPIC<->AXI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 355 subscribers
  • Views 410 views
  • Users 0 members are here
Related

AXI_MASTER_BURST 256bits IPIC<->AXI

Former Member
Former Member over 13 years ago

Hello,

When I create a new IP using AXI Burst interface, XPS creates a vhdl file (myip.vhd) with some Xilinx modules :
- the axi_lite_ipif_v1_01_a.axi_lite_ipif, to communicate with GP ports through AXI_LITE
- the axi_master_burst_v1_00_a.axi_master_burst IP, to communicate with HP ports through AXI_BURST

The thing is it seems we can't configure the axi_master_burst with more than 128 bits for the width of the IPIC interface. It's indeed confirmed in the documentation ds844_axi_master_burst.pdf. However, it's possible to have an AXI interface of 256bits.

In the documentation they also show this schema ( https://www.dropbox.com/s/j4oejn8ieohe047/256bits_IPIC.png ).
Since the "Master IPIC" is at maximum 128bits, I don't understand why it is connected with 4 HP ports (256bits). 2 HP ports could be sufficient, right ?

When I implement this design, the max frequency is about 100MHz. It means that the maximum bandwidth is 1600 MB/s (128b*100MHz) for each way. It's not that bad for the 7020 chip but can be limitating for a bigger 7045 chip with more computing power.

Is there an easy way to have a 256bits width IPIC interface to benefit of the throughput of the 4x64bits HP port (256bits) ?

Thank you for reading

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 13 years ago

    I think I will just deal directly with AXI protocol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer