Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design hello world error when creating new standalone_bsp.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 355 subscribers
  • Views 820 views
  • Users 0 members are here
Related

hello world error when creating new standalone_bsp.

Former Member
Former Member over 13 years ago

i get an error when creating new standalone_bsp, i dont know what it is can any one help me? advice or something is very much appreciated.

i'm using ISE 14.2 on windows xp.

here is the console output

make -k all
libgen -hw ../system_hw_platform/system.xml
t      
t       -pe ps7_cortexa9_0
t       -log libgen.log
t       system.mss
libgen
Xilinx EDK 14.2 Build EDK_P.28xd
Copyright (c) 1995-2012 Xilinx, Inc.  All rights reserved.

Command Line: libgen -hw ../system_hw_platform/system.xml -pe ps7_cortexa9_0
-log libgen.log system.mss


Staging source files.
Running DRCs.
Running generate.
Running post_generate.
Running include - 'make -s include "COMPILER=arm-xilinx-eabi-gcc"
"ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS= -O2 -c"
"EXTRA_COMPILER_FLAGS=-g"'.

Running libs - 'make -s libs "COMPILER=arm-xilinx-eabi-gcc"
"ARCHIVER=arm-xilinx-eabi-ar" "COMPILER_FLAGS= -O2 -c"
"EXTRA_COMPILER_FLAGS=-g"'.
"Compiling xadc"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling standalone"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -march=armv7-a -mfloat-abi=soft -mfpu=neon -I./. -I../../../include _exit.c _open.c _sbrk.c abort.c close.c errno.c fcntl.c fstat.c getpid.c inbyte.c isatty.c kill.c lseek.c open.c outbyte.c print.c putnum.c read.c sbrk.c sleep.c smc.c uart.c unlink.c usleep.c vectors.c write.c xil_assert.c xil_cache.c xil_exception.c xil_io.c xil_mmu.c xil_printf.c xil_testcache.c xil_testio.c xil_testmem.c xl2cc_counter.c xpm_counter.c xtime_l.c asm_vectors.S boot.S cpu_init.S translation_table.s xil-crt0.S, ...) failed.
make (e=2): The system cannot find the file specified.
"Compiling devcfg"
"Compiling dmaps"
"Compiling scugic"

make[1]: *** [standalone_libs] Error 2
make[1]: Target `libs' not remade because of errors.
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling scutimer"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling scuwdt"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling uartps"
process_begin: CreateProcess(NULL, arm-xilinx-eabi-gcc -O2 -c -g -I./. -I../../../include *.c, ...) failed.
make (e=2): The system cannot find the file specified.

make[1]: *** [libs] Error 2
"Compiling cpu_cortexa9"
ERROR:EDK:369 -  make failed for target "libs"
ERROR:EDK:3418 - Error(s) while running make.
make: *** [ps7_cortexa9_0/lib/libxil.a] Error 2
make: Target `all' not remade because of errors.


  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 13 years ago

    1) After SDK crashes and the BSP gets corrupted.

    No crashes of SDK

    2) If there are errors in the HW_Platform.

    The HW_platform is the solve lab 2 from the speed way hello world, so is correct.

    I think i have seen some post here in the forum somethink similar but in ISE 14.4, and on the xilinx webpage is a resolved similar isuie but for ISE 14.4 on Windows 7 x64

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    i think this is similar with my problem
    http://zedboard.org/comment/1565#comment-1565

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    I was working on ISE 14.2 System Edition
    I installed ISE 14.2 Embedded Edition and works just fine.
    Thank you all for your help! :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    I had a similar problem with ISE 14.4 in SDK, with compile errors when trying to create the BSP from the HW Platform, like others here:
    http://www.zedboard.org/content/zedboard-tutorial-problem-lab2#comment-2160

    I finally found the solution by from Kevin (zedhed) here: http://www.zedboard.org/content/problems-creating-board-support-files-zed-144-version-sdk

    The solution was Kevin's suggestion 1: 1Launch PlanAhead from a command line, then launch SDK from PlanAhead.
    Specifically, I launched PlanAhead from the u201CISE Design Suite 64-bit Command Promptu201D by typing u201Cplanaheadu201D. Then I created and exported the HW_Platform to SDK and the BSP was created without errors finally.


    But I found that Kevin's solution 2 from, starting SDK from Start menu did NOT work for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer