Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Partial Reconfiguration for the Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 347 subscribers
  • Views 1415 views
  • Users 0 members are here
Related

Partial Reconfiguration for the Zedboard

Former Member
Former Member over 13 years ago

Hi Forum,

I was wondering if anyone has managed to complete a partial reconfiguration (PR) project with the zedboard, specifically having the PL completely reprogrammed with the PS and a stand-alone OS.

So far I have managed to generate full and partial bitfiles and program the board just using impact. I fall on my face, however, when I attempt to code something in the Stand alone OS through SDK. To test I convert the partial bitfiles into bin files and use the XMD to store it in the DDR. I then found some code regarding the Zynq on the Xilinx forums for programming the fabric with the stored bin file.

Has anyone successfully managed to do this?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hi all,
    I am also trying to reconfigure the PL from soft.
    I follow the steps described in the TRM. After I initiate a DMA transfer, the D_P_DONE_INT flag is set, meaning that "Both DMA and PCAP transfers are done for intermediate and final transfers". BUT, the DONE_INT flag (which means "DONE signal from PL indicating that programming is complete and PL is in user mode") is not set.

    TRM indicates that "The PCFG_DONE flag will not be set if the previous PL configuration was not cleared using PCFG_PROG_B". But I do clear the previous config.

    Is there more steps to do to program the PL after the DMA transfer is done?
    Does the bitstream have to be wrapped somehow? I am using the same bit file as the one I use when configuring the PL with SDK->program FPGA tool.
    Is there a means to check if data is correctly transferred?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Hi all,
    I am also trying to reconfigure the PL from soft.
    I follow the steps described in the TRM. After I initiate a DMA transfer, the D_P_DONE_INT flag is set, meaning that "Both DMA and PCAP transfers are done for intermediate and final transfers". BUT, the DONE_INT flag (which means "DONE signal from PL indicating that programming is complete and PL is in user mode") is not set.

    TRM indicates that "The PCFG_DONE flag will not be set if the previous PL configuration was not cleared using PCFG_PROG_B". But I do clear the previous config.

    Is there more steps to do to program the PL after the DMA transfer is done?
    Does the bitstream have to be wrapped somehow? I am using the same bit file as the one I use when configuring the PL with SDK->program FPGA tool.
    Is there a means to check if data is correctly transferred?