Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Partial Reconfiguration for the Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 350 subscribers
  • Views 1432 views
  • Users 0 members are here
Related

Partial Reconfiguration for the Zedboard

Former Member
Former Member over 13 years ago

Hi Forum,

I was wondering if anyone has managed to complete a partial reconfiguration (PR) project with the zedboard, specifically having the PL completely reprogrammed with the PS and a stand-alone OS.

So far I have managed to generate full and partial bitfiles and program the board just using impact. I fall on my face, however, when I attempt to code something in the Stand alone OS through SDK. To test I convert the partial bitfiles into bin files and use the XMD to store it in the DDR. I then found some code regarding the Zynq on the Xilinx forums for programming the fabric with the stored bin file.

Has anyone successfully managed to do this?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Yes! It works now. Thank you zedhed.
    I've found what I was looking for on this page: http://wiki.xilinx.com/zynq-pr-rd

    The bitstream generated in PlanAhead cannot be used like that when configuring the PL through a PCAP transfer. It must be converted to a binary format. It's simply a TCL command to use:

    exec promgen -b -w -p bin -data_width 32 -u 0 yourbitstream.bit -o convertedbitstream.bin

    Note that "-data_width 32" forces the file length to be a multiple of 4 bytes, as source length and destination length are  the "Total number of 32-bit words in the PL bitstream" for a PCAP transfer.

    I haven't read entirely the link mentioned above, but it seems really interesting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Yes! It works now. Thank you zedhed.
    I've found what I was looking for on this page: http://wiki.xilinx.com/zynq-pr-rd

    The bitstream generated in PlanAhead cannot be used like that when configuring the PL through a PCAP transfer. It must be converted to a binary format. It's simply a TCL command to use:

    exec promgen -b -w -p bin -data_width 32 -u 0 yourbitstream.bit -o convertedbitstream.bin

    Note that "-data_width 32" forces the file length to be a multiple of 4 bytes, as source length and destination length are  the "Total number of 32-bit words in the PL bitstream" for a PCAP transfer.

    I haven't read entirely the link mentioned above, but it seems really interesting.