Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Partial Reconfiguration for the Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 350 subscribers
  • Views 1436 views
  • Users 0 members are here
Related

Partial Reconfiguration for the Zedboard

Former Member
Former Member over 13 years ago

Hi Forum,

I was wondering if anyone has managed to complete a partial reconfiguration (PR) project with the zedboard, specifically having the PL completely reprogrammed with the PS and a stand-alone OS.

So far I have managed to generate full and partial bitfiles and program the board just using impact. I fall on my face, however, when I attempt to code something in the Stand alone OS through SDK. To test I convert the partial bitfiles into bin files and use the XMD to store it in the DDR. I then found some code regarding the Zynq on the Xilinx forums for programming the fabric with the stored bin file.

Has anyone successfully managed to do this?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hi all !! I'm beginner with Zedboard and trying to test partial reconfiguration function on the Zedboard. My design for testing is very easy.
    - I designed counter and use the button to control the counter. Every time hitting the button, counter will increase 1 or decrease 1.
    - The counter module is the partial reconfigurable module with function count up and count down. In my design i just used PL for partial reconfiguration and Impact to download the bitstream (no PS).
    I built the PlanAhead project and generate the full bit stream and partial bit stream for the counter module. when I downloaded (by Impact) the full bit stream of count up module it works ok but when i try to download the partial bit stream to change the counter function from count up to count down, the function doesn't change. Or when i downloaded the full bit stream for count down, the counter doesn't change either, it still counts up. I try to with many configuration options (imported, implemented, promoted) but it still doesn't change from count up to count down.
    My questions are:
    1. Can i check the partial reconfiguration function on this way.
    2. What issues in may design or i misunderstood something in partial reconfiguration function.
    Please give me your suggestion. i appreciate your help a lot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Hi all !! I'm beginner with Zedboard and trying to test partial reconfiguration function on the Zedboard. My design for testing is very easy.
    - I designed counter and use the button to control the counter. Every time hitting the button, counter will increase 1 or decrease 1.
    - The counter module is the partial reconfigurable module with function count up and count down. In my design i just used PL for partial reconfiguration and Impact to download the bitstream (no PS).
    I built the PlanAhead project and generate the full bit stream and partial bit stream for the counter module. when I downloaded (by Impact) the full bit stream of count up module it works ok but when i try to download the partial bit stream to change the counter function from count up to count down, the function doesn't change. Or when i downloaded the full bit stream for count down, the counter doesn't change either, it still counts up. I try to with many configuration options (imported, implemented, promoted) but it still doesn't change from count up to count down.
    My questions are:
    1. Can i check the partial reconfiguration function on this way.
    2. What issues in may design or i misunderstood something in partial reconfiguration function.
    Please give me your suggestion. i appreciate your help a lot.