Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Computational Photography accelerator(Please Help!!!)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 349 subscribers
  • Views 263 views
  • Users 0 members are here
Related

Computational Photography accelerator(Please Help!!!)

Former Member
Former Member over 13 years ago

Hi,

I'm trying to do an computational photography application that uses FPGA as an accelerator on top of the Zedboard.


Does anyone know how do we input an image file(.ppm file) and put it in the Arm core to process? and how do we display the image file on LCD screen?

I want to extract some part of C code and run it on the FPGA, but I'm not sure how to set up FPGA/DMA transfer in XPS and the C code to handle DMA transfer.

And also, once when FPGA finishes its work, how to set up interrupt?

How to configure FPGA peripherals and how to configure Zedboard system using XPS?

Please help!!!!!

  • Sign in to reply
  • Cancel
Parents
  • jezmo
    0 jezmo over 13 years ago

    You clearly need to write an application to run on the arm to decode the incoming image file, send via some interface,ethernet usb etc and then you need to write an interface from the processor to the logic, driving an LCD is trivial, if you want me to write it for you send me a specification and ill sent you a quotation for the work ;-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jezmo
    0 jezmo over 13 years ago

    You clearly need to write an application to run on the arm to decode the incoming image file, send via some interface,ethernet usb etc and then you need to write an interface from the processor to the logic, driving an LCD is trivial, if you want me to write it for you send me a specification and ill sent you a quotation for the work ;-)