Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard Tutorial issues on vivado 2015.1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 348 subscribers
  • Views 662 views
  • Users 0 members are here
Related

Zedboard Tutorial issues on vivado 2015.1

Former Member
Former Member over 10 years ago

Hello all, I'm starting to work with the ZedBoard and as i'm going through the tutorial provided with the website. I manage to fix the first errors that I faced but right now I'm stuck in exercise 4. I've followed all the steps carefully but i can't generate my bitstream. I got the following error messages:
[Common 17-55] 'set_property' expects at least one object.It
seems to me that something went wrong on my block design (you can check it here - http://postimg.org/image/5trz6zqad/). Should I get a 16 bit vector in the IRQ_F2P entrance of my ZNYQ7 PS block? Also I can't spi_0_ss_iobuf component instaciation. any chances all this could be related? I'm running vivado 2015.1 in a windows 8.1 64bits OS

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    The issue comes up because Vivado somehow does not want to let the user type out the constraints in the XDC file.

    If you "Open Elaborated Design" in "RTL Analysis" in the flow navigator (after synthesizing your design without pin assignments), it allows you to open the IO planning layout. In this layout , you can do your pin assignments and save them. Vivado will then not give you the set_property error.
    Note, you can select the IP planning layout from the drop down layout menu on the bar below the menu bar . It will show up when you open the elaborated design.
    Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Sorry for the typo in my above post, its IO planning and not IP planning

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Sorry for the typo in my above post, its IO planning and not IP planning