Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design USB-JTAG drivers with ISE14.x/Windows7_64bit/Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 341 subscribers
  • Views 244 views
  • Users 0 members are here
Related

USB-JTAG drivers with ISE14.x/Windows7_64bit/Zedboard

Former Member
Former Member over 12 years ago

I am working with the Zedboard, ISE 14.6 and Windows7 64 bit. So far I was able to get the UART-USB driver installed working to command LED's on/off but I cannot seem to get the USB-JTAG to work. I even tried downloading Digilent Xilinx plug-in but it's not helping -- I cannot properly get the driver to work such that it can recognize and use the USB-JTAG cable... I tried manually copying the .dll's in the correct Windows folder like I did for the Cypress UART driver etc... I am doing the Speedway tutorials and am just doing the Hello World Lab2... and I am having problems programming the FPGA. There is not much out there for ISE 14.6 support...all workarounds seem to be for earlier versions. I would rather not install an earlier version but will if I absolutely have to.

Update: I did install ISE 14.2 and the same thing is happening.

Also Device manager dos not see the Digilent micro USB-JTAB cable (but does see the Cypress UART one).

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    Do you know who your local Avnet FAE is? It would be helpful if you could test a known-good working board with your system and also test your board with a known-good install. At least then you could rule out (or verify) a problem with your board.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to bhfletcher

    Well after much hair pulling I was able to just bring up Impact and do the cable auto connect (even though I never used Impact for anything ever) and after that the USB JTAG just works even if I don't ever bring up Impact. I don't understand why this works, really but it solved my problem.

    I should probably get the contact info for the AE though for future issues...