Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AD-FMCMOTCON1-EBZ Reference Design .tcl doesn't work in Vivado 2014.2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 346 subscribers
  • Views 522 views
  • Users 0 members are here
Related

AD-FMCMOTCON1-EBZ Reference Design .tcl doesn't work in Vivado 2014.2

Former Member
Former Member over 11 years ago

I have a AD-FMCMOTCON1-EBZ motor control kit for a Zedboard. I am not able to build the Vivado reference design for the programmable logic as detailed here: http://wiki.analog.com/resources/eval/user-guides/ad-fmcmotcon1-ebz/reference_hdl/linux

Supposedly you clone the github repo:
https://github.com/analogdevicesinc/hdl/tree/master/projects/motor_control

Then open Vivado and in the tcl console type:
cd [project_path]/projects/motor_control/zed
source ./system_project.tcl

It starts making a project but won't finish. This is the error:

ERROR: [BD 5-216] VLNV <xilinx.com:ip:processing_system7:5.3> is not supported for this version of the

tools.The latest version is:5.4
ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

    while executing
"create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7"
    invoked from within
"set sys_ps7  [create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7]"
    (file "../../../projects/common/zed/zed_system_bd.tcl" line 46)

    while executing
"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"
    (file "system_bd.tcl" line 3)

    while executing
"source system_bd.tcl"
    (procedure "adi_project_create" line 94)
    invoked from within
"adi_project_create motor_control_zed"
    (file "./system_project.tcl" line 5)

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 11 years ago

    The latest version supported by Analog Devices is Vivado 2013.4.   Alternatively, you could try editing the TCL scripts to work in 2014.2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 11 years ago

    The latest version supported by Analog Devices is Vivado 2013.4.   Alternatively, you could try editing the TCL scripts to work in 2014.2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to mbrown

    This answer only yields more questions... How would one edit the .tcl file to work with 2014.2 or 2014.3?

    Will my Vivado license file will work with 2013? I have some projects that I have created with Vivado 2014 that I need to keep using. Can I run both Vivado versions on my computer at the same time? Is it possible that AD will update their github to 2014 before the end of 2014, or is this a dead program to them?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to mbrown

    I think this problem is not so much related to the version, but it is related to the IP libraries on my computer. There are MANY related posts with similar problems for the FMCOMMS reference design on the AD forums, for example: https://ez.analog.com/message/156963#156963

    One answer is as follows:
    "I see you are trying to use the Zed board with fmcomms2, for that the following libraries must be built:"

    But I can't find any documentation on what it means to "build" a library in Vivado, and a google search comes up empty. What do you think he means? Do I need to buy something? Do I need to compile something? Do I need to drag a thing from one gui window to another?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    I think this is what you looking for: http://wiki.analog.com/resources/fpga/docs/hdl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mbrown
    0 mbrown over 11 years ago in reply to Former Member

    Thanks for posting.  Yes, that is a direct link to instruction for building the Vivado Libraries.

    Also, these designs are still very much alive. ADI does not post updates for every Xilinx version of tools. Instead they typically lag back a few versions.