Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Unable to connect to ps7_cortexa9
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 348 subscribers
  • Views 497 views
  • Users 0 members are here
Related

Unable to connect to ps7_cortexa9

Former Member
Former Member over 10 years ago

Hi !

I'm currently developping on a ZedBoard (Rev C) with a working design (tested). However, I haven't been able to launch any program (Hello World...) for some days and I get everytime the same error:

http://hpics.li/5ca51f4 (link to the screenshot)

Blue LED is lighting after the FPGA is programmed but it seems the programming tool can't view any ARM device. I tried with the XDM command "connect arm hw" and I obtained the following answer:

JTAG chain configuration
--------------------------------------------------
Device   ID Code        IR Length    Part Name
1       03727093           6        xc7z020
ERROR:
tCould not find a ARM device on the board. Please check if the target is in:
t 1. Split JTAG mode - No operations are possible with ARM DAP
t 2. Non Jtag bootmode - Bootrom may need time to enable DAP. Please try again


Here is my configuration:
J17: USB programmation
J14: UART
JP2: closed
JP7-JP11 : to GND (JTAG config)
VADJ: 2V5
everything else opened

I'm working with Vivado 2015.1 under Windows 8.1 (but also tested with Win7)

Do you know, guys, what is this related to ? I've already searched on forums but the answers don't work for me.

Thank you !

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    Is it possible that you damaged your board? If you damage the USB-JTAG circuit or the Zynq device, then you could get an error like you are seeing. You could try using an external JTAG cable to see if bypassing the USB-JTAG circuit helps.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 10 years ago

    Is it possible that you damaged your board? If you damage the USB-JTAG circuit or the Zynq device, then you could get an error like you are seeing. You could try using an external JTAG cable to see if bypassing the USB-JTAG circuit helps.

    Bryan