Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design UART drivers not working in Win10 Pro/Home 64bit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 352 subscribers
  • Views 3343 views
  • Users 0 members are here
Related

UART drivers not working in Win10 Pro/Home 64bit

rathseg
rathseg over 8 years ago
Hi,
 
   I just got a Zedboard and I am trying to get it up and running but I am getting stuck right at the very beginning with getting the UART connection to work.  I followed the included instructions with the board.  I got the Green Power light, blue done light, "digilent" image on the OLED, and a solid amber light on the UART LD11.  
 
I went to the next step that says you need to install the driver for the Cypress CY7C64225  USB-to-UART.  I found the the 1.3 install guide from here: http://zedboard.org/support/documentation/1521  I went to the Cypress site, got the CypressDriverInstaller_1 file and installed it.  It said it installed fine(* there are discrepancies with the install guide after install, which I will get to in a minute ).  The amber light turned off instead of blinking.  Tried reconnecting the Zedboard, turning on/off, restarting computer.  In all cases, the UART amber light is off and I cannot connect with a terminal program.
 
Compared with the install guide there are some things that are different in the device manager.  There is no device listed as "CypressUsbConsoleWindowsDriver" as Figure 4/Step 9 shows.  Under Ports ( COM and LPT ),  it is called USB Serial Port ( COM4 ), not "Cypress Serial".   USB Serial Port is the Zedboard as it only appears if I turn on the Zedboard.  Going into the properties for the USB Serial Port under Port Settings->Advanced as steps 10 and 11 indicate, there is no option for Enable Port Persist, but under "Com Port Number" dropdown box ( bottom of the picture step 11 ), there is an option for "enable RTS-DTR Flow Control" and "Other Serial Device Setup" with the option "Compatible I2C Slave Device Address (7 bit Even Address ) with 0x42 in the textbox.  USB to UART Adapter is under "Universal Serial Bus Controllers" but is not mentioned in the install guide.
 
I started checking the forums and found this post: http://zedboard.org/content/uart-driver-does-not-work-new-pc and tried ALL the suggestions there with no change.  That thread was pretty old so I thought I'd start a new one.  If I uninstall everything and turn on the zedboard I can get the solid amber light back.
 
I also tried hooking up the Zedboard to a laptop running Windows 10 Home 64-bit, with the exact same results.
 
OS: Windows 10 Pro 64 bit
USB Serial Port Version number after Cypress driver install: 3.13.0.59 dated 10/13/2105
USB to UART Adapter Version number after Cypress driver install 3.13.0.59 dated 10/13/2015
 
I'm pretty much out of ideas at this point and could use some more suggestions.  A few other details.
 
Thanks in advance.