Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design How to use Zedboard DSP multiplier, how to use Instantiation Template
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 348 subscribers
  • Views 810 views
  • Users 0 members are here
Related

How to use Zedboard DSP multiplier, how to use Instantiation Template

Former Member
Former Member over 10 years ago

Hello,

I'm new to Zedboard and even to FPGA or VHDL design.

I'm now building a project that uses the multiplier in the DSP part of Zedboard. I use Vivado 2014.4 or 2015.2

From page 56 of http://www.xilinx.com/support/documentation/sw_manuals/xilinx2014_2/ug953-vivado-7series-libraries.pdf

I found that I need to use VHDL Instantiation Template to instantiate the multiplier. These template can also found in Language Templates in Vivado.

But how to use the template? Where should I put the code in template to?

Appreciate any help. Thank you.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    What are you trying to accomplish? Is this part of a design including the Zynq PS (Processing System) or just a logic based HDL (VHDL or Verilog) design?

     

    If it is non-processor logic only design then you would include the HDL code from the template within your top level HDL code. A great way to learn how to do with within the Vivado design suite would be to attend one of the Avnet  Introduction to Vivado Speedway Workshops:

    http://www.em.avnet.com/en-us/design/trainingandevents/Pages/Introduction-to-Vivado-SpeedWay-Design-Workshops.aspx

     

    There are also some good tutorials on the Xilinx University site that target the ZedBoard: 

    http://www.xilinx.com/support/university/boards-portfolio/xup-boards/XUPZedBoard.html#resources

     

    If this is just a part of a larger Zynq design including the Processor System you will probably want to use the template to 'create' a custom IP block and use that within a Vivado IP Integrator design. The Xilinx University site linked above has workshops that target this design flow as well.

    The Avnet 'Developing Zynq SOC Hardware' Speedway workshop is available online:

    http://zedboard.org/support/trainings-and-videos

     

    Or you could start with the Xilinx Vivado Embedded Design Users Guide:

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug898-vivado-embedded-design.pdf

     

    Or one of these Xilinx Vivado Embedded Design Tutorials:

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug940-vivado-tutorial-embedded-design.pdf

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug1165-zynq-embedded-design-tutorial.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    What are you trying to accomplish? Is this part of a design including the Zynq PS (Processing System) or just a logic based HDL (VHDL or Verilog) design?

     

    If it is non-processor logic only design then you would include the HDL code from the template within your top level HDL code. A great way to learn how to do with within the Vivado design suite would be to attend one of the Avnet  Introduction to Vivado Speedway Workshops:

    http://www.em.avnet.com/en-us/design/trainingandevents/Pages/Introduction-to-Vivado-SpeedWay-Design-Workshops.aspx

     

    There are also some good tutorials on the Xilinx University site that target the ZedBoard: 

    http://www.xilinx.com/support/university/boards-portfolio/xup-boards/XUPZedBoard.html#resources

     

    If this is just a part of a larger Zynq design including the Processor System you will probably want to use the template to 'create' a custom IP block and use that within a Vivado IP Integrator design. The Xilinx University site linked above has workshops that target this design flow as well.

    The Avnet 'Developing Zynq SOC Hardware' Speedway workshop is available online:

    http://zedboard.org/support/trainings-and-videos

     

    Or you could start with the Xilinx Vivado Embedded Design Users Guide:

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug898-vivado-embedded-design.pdf

     

    Or one of these Xilinx Vivado Embedded Design Tutorials:

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug940-vivado-tutorial-embedded-design.pdf

    http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug1165-zynq-embedded-design-tutorial.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Gary, Thanks for your reply.

    This would be part of a design including the Zynq PS (Processing System).

    My design would be almost the same as the project here:
    http://islab.soe.uoguelph.ca/sareibi/TEACHING_dr/XILINX_VIVADO_dr/VivadoEmbeddedZyncTutorialAddIP.pdf

    The difference is that they design a multiplier themselves (by Create the Custom IP), but I want to use the multiplier in DSP48 of Zynq7000.

    Like you said, it seems that I should create custom IP, using the template.

    And the tutorial you post should be helpful. Thank you.