Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Interface custom VHDL code with PS simple_register
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 349 subscribers
  • Views 2103 views
  • Users 0 members are here
Related

Interface custom VHDL code with PS simple_register

Former Member
Former Member over 13 years ago

I followed the instructions to create custom peripheral simple_register. I am able to read and write values to my register.

I am now interested in connecting my VHDL entity to the simple_register inside the PS.
e.g my VHDL entity has:

entity fpga1_top_fp is
    Port (
    --! Inputs
    clk                 : in std_logic; --! clock input
    rst                 : in std_logic; --! reset
    ce                  : in std_logic; --! enable
    ndata_en            : in std_logic; --! new data enable
    ia                  : in std_logic_vector(31 downto 0);
    --! Outputs
    va                  : out std_logic_vector(31 downto 0)
    ) ;
end entity fpga1_top_fp;

Now I connect this in user_logic.vhd:
uut: fpga1_top_fp PORT MAP(
clk => Bus2IP_Clk,
rst => slv_reg0(0),
ce => slv_reg0(1),
ndata_en => slv_reg0(2),
ia => slv_reg1,
va => slv_reg2);

I have instantiated my simple_register with 16 registers and I am using slv_reg0 to set my handshaking signals. slv_reg1 is a write register and slv_reg2 is a read register.

Qns:
1. How do I add fpga1_top_fp to my synthesis path through planahead?
2. The workaround I did was to synthesize and implement my fpga1_top_fp using ISE and then copy the .ngc files and the coregen .ngc files to the .srcs/edk/implementation folder. Still I see Translate error when using PlanAhead to implement my design.
Errors:
a. BUffers of the same direction cannot be placed in series,
b. FCLK_CLK0 is driving non-buffer primitives

Any suggestions or pointers to start troubleshooting?

Thanks in advance !!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    Hi

    You need to make new ports in your user_logic and simple_register HDL files and then Rescan User Repositories and make these ports external in XPS.  Then go back into PlanAhead and edit the top level HDL to include the connections you need.  There's a useful tutorial here in the "Hardware Development Lab":

    http://www.xilinx.com/training/embedded/embedded-design-tutorials.zip

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    Hi

    You need to make new ports in your user_logic and simple_register HDL files and then Rescan User Repositories and make these ports external in XPS.  Then go back into PlanAhead and edit the top level HDL to include the connections you need.  There's a useful tutorial here in the "Hardware Development Lab":

    http://www.xilinx.com/training/embedded/embedded-design-tutorials.zip

    Matthew