Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Interface custom VHDL code with PS simple_register
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 348 subscribers
  • Views 2092 views
  • Users 0 members are here
Related

Interface custom VHDL code with PS simple_register

Former Member
Former Member over 13 years ago

I followed the instructions to create custom peripheral simple_register. I am able to read and write values to my register.

I am now interested in connecting my VHDL entity to the simple_register inside the PS.
e.g my VHDL entity has:

entity fpga1_top_fp is
    Port (
    --! Inputs
    clk                 : in std_logic; --! clock input
    rst                 : in std_logic; --! reset
    ce                  : in std_logic; --! enable
    ndata_en            : in std_logic; --! new data enable
    ia                  : in std_logic_vector(31 downto 0);
    --! Outputs
    va                  : out std_logic_vector(31 downto 0)
    ) ;
end entity fpga1_top_fp;

Now I connect this in user_logic.vhd:
uut: fpga1_top_fp PORT MAP(
clk => Bus2IP_Clk,
rst => slv_reg0(0),
ce => slv_reg0(1),
ndata_en => slv_reg0(2),
ia => slv_reg1,
va => slv_reg2);

I have instantiated my simple_register with 16 registers and I am using slv_reg0 to set my handshaking signals. slv_reg1 is a write register and slv_reg2 is a read register.

Qns:
1. How do I add fpga1_top_fp to my synthesis path through planahead?
2. The workaround I did was to synthesize and implement my fpga1_top_fp using ISE and then copy the .ngc files and the coregen .ngc files to the .srcs/edk/implementation folder. Still I see Translate error when using PlanAhead to implement my design.
Errors:
a. BUffers of the same direction cannot be placed in series,
b. FCLK_CLK0 is driving non-buffer primitives

Any suggestions or pointers to start troubleshooting?

Thanks in advance !!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    First of all, thanks a lot for the link to the tutorials. It was interesting to go through the tutorials and implement the GPIO register as a peripheral on the PS.

    So I followed the same example and started with a basic zynq PS. Then I instantiated a simple_register mentioned in ZynqGeek's blog post. I instantiated 8 of those registers in the PS ports section. Now when I generate the VHDL instantiation template I don't see any ports to connect to the VHDL logic.

    What I understand from your second post is that in my top VHDL module (in PlanAhead),
    1. I instantiate the PS with it's set of ports (no mention of simple_register),
    2. Instantiate the simple_register.vhd block and modify it to take the register value out?
    3. Connect the register port to my VHDL block.
    4. Synthesize and implement?

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    First of all, thanks a lot for the link to the tutorials. It was interesting to go through the tutorials and implement the GPIO register as a peripheral on the PS.

    So I followed the same example and started with a basic zynq PS. Then I instantiated a simple_register mentioned in ZynqGeek's blog post. I instantiated 8 of those registers in the PS ports section. Now when I generate the VHDL instantiation template I don't see any ports to connect to the VHDL logic.

    What I understand from your second post is that in my top VHDL module (in PlanAhead),
    1. I instantiate the PS with it's set of ports (no mention of simple_register),
    2. Instantiate the simple_register.vhd block and modify it to take the register value out?
    3. Connect the register port to my VHDL block.
    4. Synthesize and implement?

    Thanks!