Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design FSBL SD start error
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 350 subscribers
  • Views 1115 views
  • Users 0 members are here
Related

FSBL SD start error

Former Member
Former Member over 9 years ago

Iwant to start a standalone elf on the board,
I have imaged three files(fsbl elf, bit, standalone elf )into a bin file , and the  mode is  setted at SD_START ,  it doesn't work,

If I replaced the fsbl elf file(generated from defualt set) with the zedboard fsbl elf file ,
it works,

and now I don't why the fsbl file (generated from the default parogramme) doesn't work

who can help me ,
thanks very much!!

Xilinx First Stage Boot Loader
Release 2015.2tMar 11 2016-15:12:41
Devcfg driver initialized
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD: Unable to open file BOOT.BIN: 3
SD_INIT_FAIL
FSBL Status = 0xA009

This Boot Mode Doesn't Support Fallback
In FsblHookFallback function

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Ed,

    In our Developing Zynq Software Speedway 2016.2, we go through the steps required to create an SD card image for a Zedboard,MicroZed, and PicoZed development platform. I would like you to go through that portion of the Speedway and make sure you can replicate the example. You can find it here http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20152-and-20162 and please refer to lab07. Please use the 2016.2 toolset while you do so.

    Based on what you are saying, you have validated that the Out of Box image works on both your SD card and the SD card that came with your Zedboard. So your SD card should be OK to use.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Ed,

    In our Developing Zynq Software Speedway 2016.2, we go through the steps required to create an SD card image for a Zedboard,MicroZed, and PicoZed development platform. I would like you to go through that portion of the Speedway and make sure you can replicate the example. You can find it here http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-software-vivado-20152-and-20162 and please refer to lab07. Please use the 2016.2 toolset while you do so.

    Based on what you are saying, you have validated that the Out of Box image works on both your SD card and the SD card that came with your Zedboard. So your SD card should be OK to use.

    --Josh