Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Clock for RTL Module
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 352 subscribers
  • Views 1445 views
  • Users 0 members are here
Related

Clock for RTL Module

adamc
adamc over 2 years ago

I have a custom verilog module that I would like to provide a 100mhz clock. For the zcu102, I would normally just create a clock constraint using the si570 but I can't seem to find an equivalent on the zuboard. The constraint wizard also doesn't seem to allow for generated clocks with the zuboard. Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • adriang
    adriang over 2 years ago +3 verified
    You can use a PS2PL clock, in which case constraints are being handled by the block design containing the PS. If you do a build with that and report clocks you should see it properly constrained. As far…
  • adamc
    adamc over 2 years ago in reply to adriang +3 verified
    That worked! Thank you adriang! For those looking to do the same... 1. Go to "open block design" -> click + sign "Add IP" -> search for "ps" -> add zynq ultrascale 2. Double click "zynq ultrscale" block…
Parents
  • adriang
    +1 adriang over 2 years ago

    You can use a PS2PL clock, in which case constraints are being handled by the block design containing the PS. If you do a build with that and report clocks you should see it properly constrained. As far as I can tell there's no clock input to the PL from pins on the ZUBoard, so a regular pin+clock constraint in your xdc is not applicable.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • adamc
    +1 adamc over 2 years ago in reply to adriang

    That worked! Thank you adriang!

    For those looking to do the same...
    1. Go to "open block design" -> click + sign "Add IP" -> search for "ps" -> add zynq ultrascale
    2. Double click "zynq ultrscale" block in design -> click "clock configuration" on left -> click "output clocks" tab -> "low power domain clocks" -> configure a new clock under "pl fabric clocks"
    3. In the block design, connect the new "pl_clk0" output on "zynq ultrascale" to your RTL clock input.
    4. Run synthesis and go to I/O Ports and find your clock input pin. Then right click on it and choose "autoplace io ports". I also set mine to "Fixed" after it was autoplaced, but I'm not sure that was necessary.
    5. Use the "constraints wizard" to setup your clock.
    6. Now you should be able to generate a bitstream. Enjoy your new clock!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • adamc
    +1 adamc over 2 years ago in reply to adriang

    That worked! Thank you adriang!

    For those looking to do the same...
    1. Go to "open block design" -> click + sign "Add IP" -> search for "ps" -> add zynq ultrascale
    2. Double click "zynq ultrscale" block in design -> click "clock configuration" on left -> click "output clocks" tab -> "low power domain clocks" -> configure a new clock under "pl fabric clocks"
    3. In the block design, connect the new "pl_clk0" output on "zynq ultrascale" to your RTL clock input.
    4. Run synthesis and go to I/O Ports and find your clock input pin. Then right click on it and choose "autoplace io ports". I also set mine to "Fixed" after it was autoplaced, but I'm not sure that was necessary.
    5. Use the "constraints wizard" to setup your clock.
    6. Now you should be able to generate a bitstream. Enjoy your new clock!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer