Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Unable to use JTAG on zuboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 347 subscribers
  • Views 834 views
  • Users 0 members are here
Related

Unable to use JTAG on zuboard

kjames4
kjames4 over 2 years ago

I'm trying to use the ZuBoard for the first time with JTAG, following Lab 2 instructions.

I have a 60W usb-c power supply connected, as well as micro usb to the linux host.  The board is on, and I can see Future Technology in lsusb.  All 4 dip switches are ON, matching the configuration shown for JTAG.

I see nothing on /dev/ttyUSB0 or /dev/ttyUSB1 (both of which exist only when the board is connected and turned on).  Vitis error says can't find Arm.

All of the voltage present, power good, and micro usb LEDs in the guides are on, along with 4 red LEDs and very bright white LED near the DIP switches.  I don't see these mentioned in the docs.  Do these LEDs mean the mode is incorrect?  Is there a basic test for JTAG working?

  • Sign in to reply
  • Cancel

Top Replies

  • kjames4
    kjames4 over 2 years ago +1
    Turns out to be a driver problem. I started from Lab 1 and there are some important details in Lab 0. For anyone else missing this: tools/Xilinx/Vivado/2023.1/data/xicom/cable_drivers/lin64/install_script…
  • kjames4
    0 kjames4 over 2 years ago

    I am able to get serial output if I use the QSPI image on the board.  I'm starting to suspect that Vitis is missing drivers or permissions.  The only connection available is helpfully called "Local" and has no properties.  There is no serial console that I can find in Vitis even though I see one referred to online.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kjames4
    0 kjames4 over 2 years ago

    Turns out to be a driver problem.  I started from Lab 1 and there are some important details in Lab 0.  For anyone else missing this:

    tools/Xilinx/Vivado/2023.1/data/xicom/cable_drivers/lin64/install_script/install_drivers$ sudo ./install_drivers