Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Using the Zuboard syzygy ports
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 343 subscribers
  • Views 678 views
  • Users 0 members are here
Related

Using the Zuboard syzygy ports

loukilitarik2020
loukilitarik2020 11 months ago

Hi,

I'm trying to use a few PMODs sensors with the Zuboard, any recommendations on how to achieve that. I already bought the SZG-PMOD4 (Opal Kelly) but it didnt work for me.

Thanks

Tarik

  • Sign in to reply
  • Cancel
Parents
  • iksevas
    0 iksevas 11 months ago

    You will need to use the HSIO standard or TXR2 with PMOD voltage of 1.8V because of ZUBoard HP bank signal levels.

    The Syzygy PMOD board is looking for VIO of 3.3V which ZUboard will not provide. So either you have no voltage provided to PMOD connector if add-on card is blocking that voltage or you have 1.2V/1.8V from  ZUBoard which may not power your PMOD which requires 3.3V.

    A properly designed add-on board would require level translation to support  all of the voltages.

    You may be better off using MikroE Click to PMOD but this is IO limited so you won’t get as many PMODs..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • iksevas
    0 iksevas 11 months ago

    You will need to use the HSIO standard or TXR2 with PMOD voltage of 1.8V because of ZUBoard HP bank signal levels.

    The Syzygy PMOD board is looking for VIO of 3.3V which ZUboard will not provide. So either you have no voltage provided to PMOD connector if add-on card is blocking that voltage or you have 1.2V/1.8V from  ZUBoard which may not power your PMOD which requires 3.3V.

    A properly designed add-on board would require level translation to support  all of the voltages.

    You may be better off using MikroE Click to PMOD but this is IO limited so you won’t get as many PMODs..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • loukilitarik2020
    0 loukilitarik2020 11 months ago in reply to iksevas

    i think you are correct, it is a voltage level problem. are you aware of any expansion board with a voltage level translation for these Syzygy ports 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iksevas
    0 iksevas 11 months ago in reply to loukilitarik2020

    Unfortunately I do not.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.