Azure Sphere Starter Kit
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Blog Azure Sphere OS 19.09 - New Capabilities for your Starter Kit!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: peterfenn
  • Date Created: 11 Oct 2019 11:48 PM Date Created
  • Views 3943 views
  • Likes 10 likes
  • Comments 22 comments
  • azure sphere
  • azure sphere mt3620 starter kit
  • azure
  • sphere
  • 19.09
  • mt3620
Related
Recommended

Azure Sphere OS 19.09 - New Capabilities for your Starter Kit!

peterfenn
peterfenn
11 Oct 2019

*** Note! Updated Oct 19, 2019 ***

  • Enabled New Chip Features
  • Enhanced Wi-Fi capabilities
  • API changes
  • SDK Changes
  • Further Tips to Max-Out Your Starter Kit!

Azure Sphere OS 19.09 "major" release brings additional capabilities that are worth checking out.

  • Azure Sphere 19.09 Release Overview
  • Azure Sphere 19.09 Release Notes

image

Insights here on some of the new features you can take advantage of with your Starter Kit...

 

Enabled New Chip Features

ADC inputs and PWM output peripheral functions are now accessible from the high-level A7 user application. The Samples GitHub repository has been updated and now includes new applications that exercise these chip features.

Take a look at the following two examples:

  • ADC_HighLevelApp
  • PWM_HighLevelApp

Nine GPIOs with PWM functionality are accessible on the Avnet Starter Kit. See the table below.
eg. The utility and visual effectiveness of the five user-controlled LEDs (on GPIO4, GPIO5, GPIO8, GPIO9, GPIO10) can be enhanced by implementing PWM control of these GPIO outputs

image

Three GPIOs can be configured as ADC analog input pins on the Avnet Starter Kit:

image

ADC resolution is 12 bits. Maximum sample rate is 2 MHz.

 

Enhanced Wi-Fi capabilities

Good news is that the Wi-Fi capabilities have been enhanced in the 19.09 OS release to:

  1. Enable connection to hidden Wi-Fi networks and
  2. Provide better network discovery in congested Wi-Fi environments.

These features are supported both through the azsphere device wifi command and in the wificonfig API.

Notes!

  • When configuring Wi-Fi settings from the 19.09 command line, the --key parameter (abbreviated as -k) is now replaced by --psk (abbreviated as -p),
    eg.   azsphere device wifi add --ssid MyHotSpot --psk 12345678
  • To delete a Wi-Fi network from the stored Wi-Fi settings, the delete parameter has been replaced by forget
    eg. azsphere device wifi forget --id 0
  • A really important new feature is the availability of the optional --targeted-scan parameter (abbreviated as -t)
    eg.   azsphere device wifi add --ssid MyHotSpot --psk 12345678 -t
    This will force connection to an SSID even if this not among the SSIDs reported by a Wi-Fi scan, or if located in a crowded wireless network environment
    (Make sure to forget instances of the target SSID from list of WiFi networks currently configured, before adding an SSID with the -t targeted-scan parameter)
    More detail on this topic is available here: https://docs.microsoft.com/en-us/azure-sphere/network/wifi-including-ble#enable-targeted-scanning

 

API changes

The 19.09 Azure Sphere OS release includes several changes to the API set:

  1. Promotion of I2C and SPI Beta APIs to LTS APIs (Long Term Support)
  2. Changes to networking Beta APIs. Some previous Beta features have been replaced by new functionality. See Applibs networking.h for the networking API details.
  3. Changes to wificonfig API. See Applibs wificonfig.h for details.
  4. New event notification and event loops Beta APIs to monitor and dispatch events (High-level apps can use these APIs to request notification and defer updates)

 

SDK Changes

The 19.09 Azure Sphere SDK has also been updated, to work with the latest OS, - it now includes sysroots for four Target API Sets
In each Visual Studio project, the Target API Set (under Properties / Configuration / General) can now be set to 1, 2, 3 or 3+Beta1909

Beta APIs can change, so projects based on Beta APIs may need to be rebuilt  (with changed Target API Set) after an OS update

 

For help with command-line options or syntax, type-in the partially completed command followed by -? or --help to get context-relevant assistance

For verbose reporting in response to commands, add -v or --verbose to the end of the command entered

For documentation of the azsphere command-line tool go here

 

Further Tips to Max-Out Your Starter Kit!

 

Tips to max-out your Starter Kit hardware! (Part 1)

 

Tips to max-out your Starter Kit hardware! (Part 2)

image

  • Sign in to reply

Top Comments

  • peterfenn
    peterfenn over 6 years ago in reply to stevesmythe +3
    Steve This is because the RTApp was previously built using a Beta API set ( 2+Beta1905 ) that has now been deprecated and is not supported by the 19.09 OS To correct this requires the following: Two files…
  • peterfenn
    peterfenn over 6 years ago in reply to peterfenn +2
    PS: An alternative solution is to eliminate completely the M4 RTApp based sampling of the ADC inputs and instead move this function to the A7 HighLevelApp (from 19.09 onwards, the ADC can now be accessed…
  • agundrum1
    agundrum1 over 6 years ago +2
    I also found the updated documentation does not state that azsphere device wifi delete -id 0 has been changed to azsphere device wifi forget -id 0
  • peterfenn
    peterfenn over 6 years ago in reply to jgroman

    Specifications for MT3620 device limit the ADC input range to be from 0V to VREF
    VREF is the external voltage reference input (accessible via header on the Starter Kit) and should be 2.5V or 1.8V
    (2.5V is the maximum voltage for ADC inputs)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jgroman
    jgroman over 6 years ago in reply to skruglewicz

    skruglewicz Steve, you can connect it like this:


    Not sure what is the maximum voltage on this sensor output, but I'd expect it to be close to Vcc. I'd use 3,3V for powering the sensor then.
    If you plan to use RLCore (M4) app, AFAIK there's no information on how to set ADC reference voltage to something else than 2,5V and signal maximum measurements may get clipped. If you want to get really exact data, you'd have to use a simple resistor voltage divider between sensor output and AN input.

    image

    HLCore (A7) apps allow setting ADC reference voltage, but it is not clear what the allowed values are, so I can't comment on that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 6 years ago

    Hello Peter,

    I am trying to connect a Heart Rate Sensor that I have from another project.

    This project used the Raspberry PI and an ADC on a breadboard connected to the Raspberry PI.

     

    I would like to attach this sensor directly to the Starter kit, but can't figure out where to hook the three leads coming from the Heart sensor.

     

    the original project Is on Hackster.io at

    https://www.hackster.io/mohamedemam0/windows-10-iot-core-reading-heart-rate-pulses-e3af03

     

    Here is some information about the project from the link.

    I did get this working with IoT Core about a year ago and thought it would be a good project to try and connect it to the starter kit.

    image

    Heart Rate Sensor

    • BLACK: Ground
    • RED: Input: +3V or +5V
    • PURPLE: Signal

    So, we need to connect the signal coming from the sensor to one of the channels in our ADC. To know how to connect the ADC, here's a scheme of our IC to know the function of each leg. (I got it from the datasheet of the IC, you can google it):

     

     

    image

     

     

    Schematic

     

    https://hacksterio.s3.amazonaws.com/uploads/attachments/305795/scheme_MCIspTCn0i.png

    image

     

    Any advice would be really helpful, I am a developer that has a limited knowledge about electronics.

    I did not know how to post this request to the group.

    Regards

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 6 years ago in reply to peterfenn

    Hello Peter Again.

    I am Also going to try to access the light sensor by using the new 19.9 SDK from the a7 project.

    before I start modifying the A7 project do you have an example that I can use?

    Otherwise I'll try and take the function from the A4 level and Place it in the A7 level.

    Any help with this would be greatly appreciated.

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skruglewicz
    skruglewicz over 6 years ago in reply to peterfenn

    hello Peter

    I'm trying to Cmake the A4 project per your instruction in the advanced project.

    I'm was able to make it but have since upgraded to os 9.10 and SDK 9.10 and vs2019

    and am now getting errors when trying to make.

     

    Severity Code Description Project File Line Suppression State Suppression State

    Error CMake Error: CMAKE_C_COMPILER not set, after EnableLanguage

     

     

    Severity Code Description Project File Line Suppression State Suppression State

    Error CMake Error at C:/Program Files (x86)/Microsoft Azure Sphere SDK/CMakeFiles/AzureSphereToolchainBase.cmake:34 (MESSAGE):

      Variable AZURE_SPHERE_TARGET_API_SET is not set.  Variable

      AZURE_SPHERE_TARGET_API_SET is not set correctly.  Set this variable to one

      of the available API sets: ["1", "2", "3", "3+Beta1909"].  To do this, use

      CMakeSettings.json (if using Visual Studio), .vscode/settings.json (if

      using Visual Studio Code), or -DAZURE_SPHERE_TARGET_API_SET=<value> (if

      using command line build). C:/Program Files (x86)/Microsoft Azure Sphere SDK/CMakeFiles/AzureSphereToolchainBase.cmake 34

     

    Is this  Visual Studio thing?

    How do I "set,C_COMPILER after EnableLanguage"

    I'm not use to CMAKE. And it looks like I will need to know a little more about it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>