I use Azure starter kit Rev2 board and I am using the External MCU update program. I have mixed both Azure IOT and External MCU program.
There's a function "ProgramImages(images, imageCount, &DfuTerminationHandler); " in External MCU . I want…
I use Azure starter kit Rev2 board and I am using the External MCU update program. I have mixed both Azure IOT and External MCU program.
There's a function "ProgramImages(images, imageCount, &DfuTerminationHandler); " in External MCU . I want…
I'm having a hard time finding out how to receive the starter kit for free. I'm from the USA. Is the time to sign-up over?
Hi, I am having issues with I2C data reading. The code stops at "Log_Debug(buf[i]);" with a "Segmentation fault occurred".
int main(void) { static int i2cFd = -1; const uint8_t* buf[] = { 0, 0 }; Log_Debug("Loading\n"); i2cFd =…
Trying to do the daily "Azure Sphere Starter Kit Sync with Contest Server" thingie
Today when I tried to connect to the contest page, I got "WiFi not configured". So I tied to enable/disable the definition. Also a restart as well. After all this I am left with the following:
SSID : ****************
Configuration state : temp…
Hi Everyone,
I'm working on a use case that requires two high-level applications to run simultaneously. I have confirmed that I can do this utilizing the "partner application" functionality. However, in my use case I require that each application can communicate…
I am new in iOT. Right now I am working on supply chain project. We need a integrate Wifi, Sensor, REFID etc . Is this Azure Sphere is ready for production?
Azure Sphere – How to generate Leaf certificate?
It is easy to connect first device to IoT Central. There is step by step. By I want to connect second Azure Sphere device to IoT Central. It is added automatically, just because it is in Azure Sphere Tenant…
I didn't get any code. How do I get the code for free starter kit?
I have a problem, I just can see the orange "Buy Now" button, not the "Register for a free kit" button.
I am from Austria. What should I do.
Thanks for your help!
I was able to get through all the steps of the Azure Sphere setup, up until I need to connect to wifi to get the device updated. I am in a locked down corporate environment, and need to use a phone hot spot for development. I am on the latest version…
What is the maximum current the MT3620 GPIOs pins can output?
All the pis provide the same current?
Can you configure any of the pins to have high drive strength (i.e 20-mA)?
So i have been playing around with the Kit a little and i find it quite difficult to find any documentation whatsoever.
I pulled the GPIO sample application from
https://github.com/Azure/azure-sphere-samples/tree/master/Samples/GPIO/GPIO_RTApp_MT3620_B…
I am sorry to inform you that my Starting kit MT3620 Azure Sphere board stopped working.
I was able to ping every day for three days.
During this time, I worked out several examples from online tutorials.
Using the Oled display based on the advanced tutorial…
After hours of installing/uninstalling Visual Studio 2017, Azure Sphere SDK, creating Azure acount and tenant,last night a managed to load the example from Avnet first part tutorial. But in the output window it shows me that it failed to find the lms22hh…
Hello Everyone,
So far I was able to get the kit and the software installed and I was able to create the necessary accounts. Now I am facing an error that I don't know how to address. I am trying to run the reference design following the steps in this…
Using the sk_server_registration utility I am getting "Device not connected", but if I run the azsphere utility to check my connection it is successful.
Will this impact my challenge status or am I OK?
.
C:\Users\elvis\Documents>azsphere device…
Hi,
I am new to Avnet's Azure Sphere. I have executed the steps defined here:
Avnet's Azure Sphere Starter-Kit (Out of Box Demo) Part 1 of 3
After running the code in Visual Studio, the output displays around 10 Celsius degrees higher temperature…
I had been going through this sample https://www.element14.com/community/groups/internet-of-things/blog/2019/08/01/azure-sphere-starter-kit-advanced-tutorial
Everything worked in the end. let the device on all night, sending data to IoT Central successfully…
I have recently received an Azure Sphere MT3620 starter kit and have been going through the steps to get it started. However I soon had an issue where, when performing a lot of different operations I would get the message:
"error: The device is not responding…
Just after I click Send to Server I receive:
---------------------------
URL response Fail!
---------------------------
{"cpId":"RkNGOTRGQjYtMUM5RS00M( cut )","uniqueId":"hacksterSphere","data":{"emai(…
I'm a novice in C and in embedded programming. Let's say I started with Azure Sphere as there was an occasion to enter to this field in a cheap way. As a training I have successfully accessed the readings from gyro and accelerometer, but having issues…
hi have a mix of wifi and network cameras and a high quality wifi alarm is it poss to link them together? or can i use this end gadget to finally link my alexa to my bedroom fan