Freedom development platform
  • Products
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Forum Prototype shield for the Freedom Board?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 9 subscribers
  • Views 3517 views
  • Users 0 members are here
  • freescale
  • freedom_board
  • freedom
Related

Prototype shield for the Freedom Board?

fustini
fustini over 12 years ago

Hello, I was chatting with Community member, Kuya.Marc , and he is looking for a prototyping shield for the Freedom Board.  Anyone know of any?

 

thanks,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to FreescaleTools_and_Software +1
    ?? a prototyping board with dual row headers to get access to all the FRDM pins Yes A prototyping board that gave access to all the pins would be should be available in order to compliment your excellent…
  • DAB
    DAB over 12 years ago

    Hi Drew,

     

    As I recall, wasn't the Freedom board Arduino hardware compliant?

    If so, any Arduino shield should work.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to DAB

    Back in April Joe Alderson put me onto this

    http://nz.element14.com/digilent/protoshield-uno/board-protoshield-for-chipkit-uno32/dp/2311267?COM=e14_element14

     

    Not sure if the same code (2311267) matches in every store.

    Hi Mark - how about this for a protoshield?

    http://nz.element14.com/digilent/protoshield-uno/board-protoshield-for-chipkit-uno32/dp/2311267

    It doesn't quite cover all the header pins on the Freedom Board (it was designed for the chipKIT) - you would be missing the PTB8 - 11 pins and PTE2 - 5 but otherwise it accommodates the double headers.

    Cheers,

    Joe

     

    It is a shame there isn't a board that utilises/makes available the other pins, and at a reasonable price.

     

    I have a plan, for one but haven't had time to do it.

    So if someone is handy with pcb skills that is happy to come some arrangement ... let me know.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 12 years ago in reply to mcb1

    Hello Drew

    Element14/Farnell has bundled the FRDM-KL25Z with an Arduino proto shield some LEDs, Connectors, Resistors. The part number of this kit is : FRDMKL25Z PROTO BUNDLEFRDMKL25Z PROTO BUNDLE

    Arduino Proto shield can be bought separatly, its part number is : A000082A000082

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to FreescaleTools_and_Software

    Mr Freescale

     

    The Arduino offering is great but there are few boards available that connect to all the pins.

    This is a shame as the board has more to offere than just the Arduino pins.

     

    The board pricing is great, and with the addition of the headers is very good value, yet the basic shield offerings are more than the board.

     

    What plans does Freescale have for shields?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to mcb1

    Any chance Freescale are there??

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 12 years ago in reply to mcb1

    As far as I know, Freescale has no plan to launch its own shields but some of our partners might do it.

    Freescale will focus on the MCU board with its Freedom development platform for its Kinetis family ARM Cortex-M based

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to FreescaleTools_and_Software

    Thanks

     

    I have to say that is a shame, since the other offerings don't cover all the available pins/headers, making it not as useful.

     

    A simple prototyping board would be a start

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 12 years ago in reply to mcb1

    Hello Mark

    Thank you for your constructive feedback.

    Just to be sure that I understood your request, could you confirm that it could be usefull to get a prototyping board with dual row headers to get access to all the FRDM pins, right ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to FreescaleTools_and_Software

    ??

    a prototyping board with dual row headers to get access to all the FRDM pins

    Yes

    A prototyping board that gave access to all the pins would be should be available in order to compliment your excellent boards.

    This is an example of a simple low cost one for Arduino (Freetronic protoshield)

     

    It could be simply offered as a bare board and then users could choose to fit headers in order to stack, or pins in order to construct on the board.

     

    The offerings from others don't give access to all the pins on the Freescale boards.

    They are nearly twice the price of the entire board, which could mean that another platform is choosen.

     

     

    Using an Arduino shield (prototype or otherwise) removes access to all the inside ones.

    I also have an idea that would allow the use of two Arduino shields, that I'm happy to discuss ... but not in the forum.

    If you are interested then please PM me.

     

     

    Thanks

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jeandavis
    Jeandavis over 4 years ago

    The Proto Shield makes it simple to create unique circuits. You can solder parts to the prototyping service area to build your project, or you can use it with a small solderless breadboard (not supplied) to quickly test circuit ideas without soldering. It has additional connections for all of the Arduino I/O pins, as well as space for through-hole and surface mount integrated circuits. It's an easy method to combine your custom circuit and an Arduino into a single module.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>